STM32 MCUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can't get UART Loopback to work

Context:Coming from an arduino background, I wanted to further develop my MCU skills and also learn how to read datasheets and reference manuals more efficiently, so I got a NUCLEO-F767ZI board and my idea for a first "project" was to loopback UART ...

HPont.2 by Associate
  • 378 Views
  • 1 replies
  • 0 kudos

In the STM32G031 do you need to set any pins a certain way to be able to reprogram the chip with ST-LINK or with the Bootloader?

I had PA13 and PA13 set as a GPIO. I was able to program it one time with both the ST-Link V2 Clone, a.k.a Blue Pill, and via the Bootloader program stm32flash (on SorceForge.net) using the UART.Both would only work on a new chip. Once the chip was...

KiptonM by Lead
  • 869 Views
  • 10 replies
  • 0 kudos

Resolved! [RESOLVED] VCP on ST-LINK v3 mini

I cannot get the VCP function of ST-LINK v3 mini working.Windows sees the com port and can open itConnected TX output of UART to pin 14 of ST-LINK 3 mini, but nothing is received on the PC side.Connected some other serial TTL-USB adapter (set to 3.3V...

Pavel A. by Evangelist III
  • 1028 Views
  • 4 replies
  • 0 kudos