2024-07-30 2:34 PM
Arkadaşlar üzerinde bir adet MCU (32f103 v8tb) var, içindeki firmware'i okuyup başka bir karta kurmam gerekiyor. Bunu hangi st link ile yapabilirim lütfen yardımcı olun.
2024-07-30 2:42 PM
the end will be vbt6
2024-07-30 2:47 PM - edited 2024-07-30 2:53 PM
>>Friends, there is a MCU (STM32F103VBT6) on it, I need to read the firmware inside and install it on another board. With which ST-LINK can I do this, please help.
If the STM32 is not protected you can read via the SWD/JTAG connection, ie PA13:SWCLK, PA14:SWCLK, GND, and VCC/VTARGET(Pin1)
STM32 Cube Programmer can read and save content to a file, either .BIN or .HEX
Read from 0x08000000, Size 0x20000 (128KB)
Then move to destination device, an from programming tab/pane set the address and select the file and the program, and optional verify.
Protected devices (Read Out Protection) will preclude the recovery of a firmware binary
ST-LINK/V2, V2-1 or V3 would work for STM32F1 devices. ST-LINK Utility would also work for them, if the interface is easier to navigate
2024-07-30 2:48 PM
You can Edit your own posts via the small (V) icon in the upper right corner of the post.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.