STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB host disconnect automatically

Hi,We are designed board using STM32F207 for USB host. I have 2 keyboard. one keyboard work perfectly & other keyboard also work but after few second automatically disconnect from host & connect it again. Same keyboard work perfectly with STM32F407Di...

0693W000004JLMgQAO.png
RDals.1 by Associate
  • 388 Views
  • 0 replies
  • 0 kudos

Resolved! Ethernet in new STM32H73x (H72x)

Is the ETH IP in these new MCUs same as in H753/743, or changed?In the errata for H73x/72x, list of ETH related items is quite long - is it because of difference in the IP, or better testing?-- pa

Pavel A. by Super User
  • 718 Views
  • 2 replies
  • 0 kudos

Resolved! NUCLEO-F746ZG Nucleo board's (STM32F103CBT6 controller used for ST-Link) ST-link USB bootloader and programming file (.out file)

Hi,STM32F103CBT6 controller is used as "ST_link controller" in NUCLEO-F746ZG Nucleo board.I'm looking for NUCLEO-F746ZG board's ST-link USB bootloader and programming file (.out file) for STM32F103CBT6 controller. Can someone send me link/path for ST...

S.Kamath by Associate III
  • 1016 Views
  • 6 replies
  • 0 kudos

Resolved! Clock speed stm32f429i example package

Dear ST Hello,could you tell me please the real clock value set in this example,\STM32Cube\Repository\STM32Cube_FW_F4_V1.25.1\Projects\STM32F429I-Discovery\Examples\SPI\SPI_FullDuplex_ComDMAThe clock frequency between master and slave must be equal, ...