STM32 MCUs Embedded software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f429ı_dısco not written sdram

hello i have stm32f429i-disco card. fmc settings are configured. i defined sdram in the linker file but variable sdram is not written. can you help me? i am using cubeide. my linker file is attached and i am attaching the photo of my fmc settings. my...

Ekran görüntüsü 2025-05-07 223050.png
edramden by Associate II
  • 75 Views
  • 4 replies
  • 0 kudos

MIPI-DSI LTDC configuration lcd

Hello everyone, I need help with a DSI + LTDC configuration.I'm working on a custom board with an STM32H747BIT and trying to drive a 720x1280 RGB888 display without GRAM, using the ILI9881C controller via DSIHOST + LTDC.Here’s the situation:I’m curre...

LWIP & FreeRTOS - code getting stuck

Hi allI am trying to make project on LWIP & FreeRTOS on STM32f407vgtx board issue what I am facing is when code is getting stuck and no task is hitting .I am sharing my project can you please check once .note: in task I am have called Lwip_Init in my...

Ash1 by Associate III
  • 78 Views
  • 2 replies
  • 1 kudos

Time-based input capture

Hi all, I have an application where I'm trying to use input capture to capture pulse intervals in a specific period of time.  At maximum, the pulses will happen frequently enough that I can't use the straight interrupt capture with HAL_TIM_IC_Start_I...

Eclipse Threadx

I have a project (STM32H7) using Eclipse ThreadX 6.4.0. I would like to use the safety certified version of ThreadX (6.4.2). How would I go about this transition? Is there an application note covering this subject? Thanks, Gil

Gil1 by Associate II
  • 158 Views
  • 1 replies
  • 1 kudos