STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F769 USB FS Pin PB13 Question

Posted on September 21, 2017 at 20:09Taken from the datasheet  Pg. 190 (attached) 'When VBUS sensing feature is enabled, PA9 and PB13 should be left at their default state (floating input), not as alternate function. A typical 200 ?A current consump...

Kevin Wu by Associate
  • 1841 Views
  • 0 replies
  • 0 kudos

STM32L0 HAL_SPI_RECEIVE unexpected clk generation

Posted on September 18, 2017 at 17:02Hi all,First time programming with STM32 MCU. I'm using STM32CubeMX V4.22.0 with STM32Cube_FW_L0_V1.9.0. I'm trying to get 16bits ADC value with HAL_SPI_RECEIVE call and got a very strange behavior :1st call : OK...

Thomas LB by Associate III
  • 759 Views
  • 1 replies
  • 0 kudos

Noise in headphone output

Posted on September 14, 2017 at 13:50I'm using STM32f4-Discovery board for an audio application.I'm using the onboard codec CS43L22, in analog passthrough mode. But I'm getting high frequency noise on the output over headphones.Can anyone tell what ...

aditya by Associate II
  • 3210 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F4 USB serial number not unique!

Posted on September 18, 2017 at 09:27On the  different STM32F4 Discovery boards with STM32F407 that we have here the serial number of the USB Virtual Port connection, as reported on the PC, is always 00000000001A.Is this as it should be? Also, stran...

Sietse by Associate III
  • 1967 Views
  • 2 replies
  • 0 kudos

USB virtual com device(STM32F765ZI Nucleo)

Posted on September 14, 2017 at 18:45Hai., I am using STM32F767ZI NUCLEO board(144 pin), In this I need to use Full speed USB as Virtual com port device, I generated code using http://www.st.com/content/st_com/en/products/embedded-software/mcus-embe...

Nucleo F767ZI lwip and Hal interaction

Posted on September 16, 2017 at 00:24Greetings , I'm figuring out LWIP and the Ethernet setup on the above mentioned board. I've found the LWIP application note very useful in understanding LWIP and  Cube MX does extremely well to explain how to set...