STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1324 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 529 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! How to get CubeMX Capability(.ioc) for STM32CubeIDE Projects Converted from System for Workbench Projects under STM32H743I_EVAL Example Projects?

We are using STM32H743I_EVAL boards. I have gone through number of examples from "STM32Cube\Repository\STM32Cube_FW_H7_V1.6.0\Projects\STM32H743I-EVAL\Examples" folder. None of these examples seems to be for STM32CubeIDE. STM32CubeIDE does seem to kn...

BGeor.1 by Associate III
  • 2125 Views
  • 2 replies
  • 2 kudos

Using a OC timer as a DMA request.

I am trying to implement a DMA transfer as outlined in AN4666. I am using STM32CubeIDE and an STM32F4 Discovery. This will eventually let me pull data from the input register of a GPIO port (and read a parallel data stream), but for starters, I'm ju...

MCiuf.1 by Associate
  • 1847 Views
  • 2 replies
  • 0 kudos

Resolved! CubeIDE update unsigned?

When updating CubeIDE on WIndows 10 it shows the following warning. Is this normal or something bolted up? -- pa

Pavel A. by Super User
  • 1288 Views
  • 1 replies
  • 0 kudos

I am unable to debug code with enters STOP mode when the options bits are set to NOT assert reset on entering STOP mode.

With STM32CubeIDE Version: 1.0.1 Build: 3139_20190612-1256 (UTC), and an H743 Nucleo with V2J35M26, I am unable to debug code with enters STOP mode when the options bits are set to NOT assert reset on entering STOP mode. I have the registers set to k...

IAbbo.1 by Associate
  • 806 Views
  • 0 replies
  • 0 kudos