STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1359 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 537 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Bug with "STM32 Project from STM32CubeMX .ioc file"

Being able to create a new project from an existing .ioc file is very useful. But when I've tried to do this (by selecting File->New->STM32 Project from STM32CubeMX .ioc file) the project seems broken. I can build it fine, but when I try to add new (...

0693W000000UwDDQA0.png

How to copy project from STM32cubeide?

I am using STM32cubeide 1.3.0, and I am running a project called 'test_1'. I want to create a 'test_2' project based on the 'test_1' project, what should I do? I've tried several methods, but I got an error.I tried changing the name of the 'test_1' p...

Snam.1 by Associate
  • 684 Views
  • 0 replies
  • 0 kudos

Bug Creating USART2, USART3 ..... under LL

Hi when I create the USART2 and USART3 under LL using DMA the fieldGPIO_InitStruct.Mode = LL_GPIO_MODE_FLOATING;and will beGPIO_InitStruct.Mode = LL_GPIO_MODE_INPUT;the USART1 work finethanks

STM32CubeIDE V1.3.0 "Debugger connection lost"

I have seen this same thread somewhere before, but for a MAC platform, so hopefully someone has solved it for windows also.V1.3.0 Windows (running on 10) allows for .ioc creation and compiliation (using gcc eclipse compiler) but.... with both Nucleo-...

Sjohn.2 by Associate
  • 1401 Views
  • 2 replies
  • 0 kudos

STM32F429 project error: No such file or directory

Hello, I'm getting started with stm32f429i. I built my project like the picture. The problem is when i build target, I had an error like the picture.I Crtl+left click to the "stm32f4xx_sai.h" and it pop out When i rebuid target it have the same error...

0693W000000UlhWQAS.png 0693W000000Uli0QAC.png
NHuy.1 by Associate
  • 1528 Views
  • 1 replies
  • 0 kudos

CubeIDE Rendering issues on Linux (SOLVED)

I have some annoying rendering issuse with CubeIDE 1.3 running on Ubuntu 19.10 (Pop_OS).The problem is that some of the toolbox windows are not updating/re-rendering when switching tabs or perspective.Debug perspective seems to have most issues, see ...

Blem.1 by Associate
  • 1701 Views
  • 1 replies
  • 0 kudos