STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1424 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Load and start a programm in RAM with USB DFU

Hi,we try to load a small program to RAM area starting from address 0x20008000 with STMCubeIDE and USB DFU and select start address 0x20008000 ( In debugger we can see that program is load to 0x20008000).The download is successful, even so setting st...

clkr by Associate
  • 2715 Views
  • 4 replies
  • 0 kudos

Login to ST jxBrowser Window broken

When I try to login to the ST Acccount, the login window is responsive for less than a second. Than the cookie banner pops up and starts to flash (border popping up), rendering the complete window unresponsive. Eventually the cookie banner completely...

mo_krauti by Associate III
  • 761 Views
  • 3 replies
  • 0 kudos

Resolved! I can't install ide cube on ubuntu 24

When I try to install it I get this error: "The following packages have unmet dependencies:st-stm32cubeide-1.16.1 : Depends: libncurses5 but is not installableDepends: libpython2.7 but is not installableDepends: libwebkit2gtk-4.0-37 but is not instal...

Resolved! on H7A3 no SAI configuration in Cube - Bug report

Hi,big surprise: when activating SAI on H7A3ZIT , no configuration possible : ...nothing to configure...+ on IDE 1.18.0 , with newest Cube package: 1.12.1+ on H743ZIT , looks as it should:... V1.12.2  coming then ?  - or "manual setting needed ? on H...

AScha3_0-1743152470796.png AScha3_1-1743152583100.png AScha3_2-1743152726732.png
AScha.3 by Super User
  • 2260 Views
  • 5 replies
  • 0 kudos

STM32 Nucleo h745zi-q: USB-Device not recognized

Hey im currently trying to use the CubeIDE to create a simple USB COM Communication. I used the following settingsSystem CoreRCC: HSE = Crystal\Ceramic Resonator ConnectivityUSB_OTG_FSMode: Device_OnlyVBUS: DisableNo Activate_SOFSpeed: Fullspeed 12Mb...

carlo3_2-1744724943149.png carlo3_3-1744724996192.png
carlo3 by Associate
  • 1060 Views
  • 2 replies
  • 0 kudos

I want to generate a pwm pulses for up down mode

Hi everyone I am new to STM32CubeIDE and I'm trying to generate PWM pulses with a fixed duty cycle and frequency using the up-down counting mode. However, I couldn't find an option in the Timer configuration to specify the output action based on whet...

Screenshot 2025-04-15 125720.png