STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 222 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

LoRa Implementation

Hello, I am using STM32L152RE board and Hoperf RFM95 LoRa Module..So can you guide me through this..? It will be helpful if I get some libaries for this.Thanks and Regards,Umesh

i can’t debug B-L072Z-LRWAN examples with SW4STM32

Hello,I have two B-L072Z-LRWAN1 development kits. I downloaded I-CUBE-LRWAN which is LoRaWAN software expansion for STM32Cube.Normally I practice with TrueStudio . However, sample file haven’t any example for this IDE. Then, i downloaded SW4STM32. Ev...

Bug in LoRaWAN software expansion for STM32Cube

I am using V1.1.5 of the LoRa software expansion for STM32Cube and have come across an issue which leaves the stack unusable until reset.Although the problem was first encountered in our application project, I verified that the problem also occurred ...

Does anyone have a complete .IOC file for this discovery board?

Hi, I haven't found a .IOC file for the B-L072Z-LRWAN1 discovery board -- has anyone created or found such a file. I would like to use the STM Cube L0 to generate initialisation code but I need an IOC file for that. I have been looking at the intiali...

bed by Associate
  • 859 Views
  • 0 replies
  • 0 kudos

I-NUCLEO-LRWAN1 compatible boards?

Hi,I have two boards that I would like to use with the I-NUCLEO-LRWAN1 expansion board:NUCLEO-F411RE and NUCLEO-L152RE.Is any of them compatible with I-NUCLEO-LRWAN1?Thanks.

bdaniel7 by Associate II
  • 1524 Views
  • 4 replies
  • 0 kudos