STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 235 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4077 Views
  • 0 replies
  • 3 kudos

Set a GPIO using BLE sensor app

In addition to turning the Blue Led on with the p2p server app, I want to turn a Led on connected to a GPIO, using the same signal.

Hpena by Associate II
  • 1278 Views
  • 1 replies
  • 0 kudos

Use computer Bluetooth connect to STM32WB board,need PIN

I want use computer Bluetooth to communicate with STM32 board .First, I use ST BLE sensor, succeed.second,use conputer to connect,I need to write PIN.Last,I use labview to scan ,I cannot find it.​I want to set up a route from stm32WB to my PC base ap...

0690X00000AsPxfQAF.png 0690X00000AsNqmQAF.png 0690X00000AsNqrQAF.jpg
zxin.2116 by Associate II
  • 2373 Views
  • 4 replies
  • 0 kudos

Making STM32WB Discoverable

I'm working to complete the port of BlueNRG code to the STM32WB. I've gotten everything working up to the point where I make the device discoverable. The WB stack is returning an error, but there's no documentation to explain what this error could me...

eleventen by Associate III
  • 1199 Views
  • 1 replies
  • 0 kudos

Resolved! Lora - Sticky Mac commands / sheduled uplink

Hi there,I am working on Murata cmwx1zzabz (i.e. STM32L072CZ) and my code is based on the ST en.i-cube_lrwan. For all the basic stuff (joining, sending messages) it runs fine. The Mac commands, that actually manage the network, are OK except the "sti...

Bezac by Associate II
  • 1832 Views
  • 1 replies
  • 0 kudos