NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello,I'm trying to figure out why setting the MTU stops the ACI_ATT_READ_BY_GROUP_TYPE_RESP_VSEVT_CODE event from ever firing. This essentially breaks everything.case HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE: /* USER CODE BEGIN EVT_LE_CONN_COMPLETE ...
where do I get API documentation for firmware OTA of STM32WBA52CGUX ?
Hello, I designed a board based on the STM32L031F6P6 with an sx1262 chip, and it worked well using the driver https://github.com/Lora-net/sx126x_driver for LoRa transmission. I'm trying to send LoRaWAN signals, but I'm having trouble finding exampl...
Hello, I'm very new to BLE. I'm following STM example code.I want to be able to run on battery and turn on the BLE to advertise for 5 minutes then stop. After an interrupt, I want to be able to turn on advertising again.In the STM32WBA Bluetooth® LE ...
I am using stm32wle5jc ( LoRa Wio E5 mini board) with stm32wl FW stack. I tried lot ways to implement the RTC Alarm B (in BIN, MIXED and BCD mode). But is stops entire LoRa Process. How I fixed that?
I want to add a custom BLE service in STM32CubeMX. I saw on a website that the Add Custom Service feature could be used for this. However, I don't know the procedure for adding a service using this feature. Please tell me the steps to add a service u...
Hello,I am using P-Nucleo-WB55. I have made a simple BLE server example that receives data from a client and it's working well. But whenever I add sequencer tasks, while these tasks are running, if I send any data from the client (ST BLE App), the nu...
If LPAWUR, Sigfox, and Tiny_LPM are enabled in PWR_DEEPSTOP_RTC example code, will the RTC wakeup mode and DeepStop mode work properly?
I would like to know why 2 is added to the P2PNotifyServerToClientCharHdle while checking for an attribute handle match in p2p_stm.c file. Later in the same function, 1 is added to P2PWriteClientToServerCharHdle. Is there an implicit assumption made ...
Hi , I am trying to measure the output return loss ( in tx mode) of my board rf chain which include the stm32wle5.if i understnad correctly - in order to do that i need to put the STM32WLE5 in TX MODE which means its PA should be powered up and read...