STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

How to configure Lora CLASS A RxWindow. I have configured MAX_RX_WINDOW in RegionEU868.h but it is not getting reflected and in CLASS A Rx1 and Rx2 slots getting closed with in 100 msec

1081s730:MAC txDone<CR><LF>02-05-2021 23:17:35.489 [RX] - 1082s751:RX_1 on freq xxxxxxxxx Hz at DR 0<CR><LF>1082s958:MAC rxTimeOut<CR><LF>1083s715:RX_2 on freq xxxxxxxxx Hz at DR 2<CR><LF>02-05-2021 23:17:36.528 [RX] - 1083s791:MAC rxTimeOut<CR><LF>

AJ.2 by Associate II
  • 962 Views
  • 0 replies
  • 0 kudos

Workshop code insertion and BLE custom names

Hi, Working with FW_WB_V.10.0, have a few questions:After viewing the workshop tutorial, I saw multiple code insertions to the project. (https://www.youtube.com/watch?v=zNfIGh30kSs). Are they necessary?Started working with FW_WB_V.10.0, can I safely...

DS.4 by Senior II
  • 723 Views
  • 0 replies
  • 1 kudos

STM32WB stuck in sequencer

I have a custom board with a STM32WB55 that is getting stuck in the sequencer and stops executing as soon as I start my code. I can't tell if it's a race condition and I don't have the ability to step through the code with a debugger. The code is bas...

DPars.2 by Associate III
  • 908 Views
  • 0 replies
  • 0 kudos

why use TCXO, effect of not using TCXO for 32MHz?

I have read different articles of STM and received different mails to use TCXO to give 32MHz clock. I could not find the reason and impact of it. In my application, it is outdoor and able to go temperature upto 85C temperature and using 22dB with 865...

Aagra.11 by Associate II
  • 2577 Views
  • 5 replies
  • 0 kudos

STM32WL and generic packet format

Hello,I have read the datasheet/reference manual on stm32WL generic format, i also looked into the cube wl sources. From the source codes i understand that stm32wl integrates semtech sx162x radio. I have not been able to pinpoint anything more specif...