NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I'm new to STM32WB and using BLE_MeshLightingPRFNode example. With the function BLEMesh_CustomBeaconReceivedCallBack, I get the data and data is true but RSSI is wrong How can I fix it or other way to get RSSI from beacon? Sorry for my bad english Re...
I am tying to develop an application in Zephyr for a battery powered device that goes into STOP2 mode for low power consumption when advertising. I have successfully created a test app with STMCube based on the health thermometer example which does t...
Hi! We have a working project on the STM32WB55 nucleo board that we are ready to port to our target hardware which uses the STM32WB5MMG. However, the BLE portion of the project is not behaving the same. Specifically, it will advertise, but will not ...
My device is the slave, that is being connected (not always in the same order) by 2 masters.I would like to create two different connection ways/points to distinguish between the masters.MASTER1 will always connect through "way1."MASTER 2 will always...
So im trying to follow the 1:20h tutorial about how to setup BLE,narrated by ringo start's voice and i reach the part in which he refers to an inexisting .pdf file containing the links for info about HSE calibration.As cant find that .pdf he is refe...
Looking for a list of all possible commands/scenarios where CPU2 sends commands to CPU1(APP). I saw one specific case in AN5289 command during INIT, what are all the other cases?Any examples/ Further documentation will be great.
Hi,I try to set FUOTA with FREERTOS on NUCLEO-WB55 demo board.I start with the BLE_HeartRateFreeRTOS, I built it, flash it and all is ok.Then I flash OTA bootloader (I know it's working also cause I try to update with BLE_p2pServer_ota project and it...
Would like to have a better understanding on the IPCC memory manager channel.(Have read the AN5289 notes)Appreciate If you can shed more light on it.What is it purpose?Why do we have to clear it after some events?What are its memory parts purpose ? a...
Hi All, I'm currently working on a project that uses the STM32WB5MMG module.I did a porting of one of the examples of the repository (BLE_Zigbee_Dyn) for RTOS and everything is working fine.Now I'm trying to put the MCU in STOPMODE2; a GPIO Interrupt...