STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Resolved! Debugger VERY sensitive to shutting down??

I am using an STLINK-V3SET programmer / debugger. I connect to my target (STM32WB55) on a Midatronics Sharky Mkr board. I find that if I 'blink' or move funny the debugger after connecting shuts down and displays the following under the console win...

SWenn.1 by Senior III
  • 1339 Views
  • 1 replies
  • 0 kudos

Unable to successfully load BLE firmware because of FUS_IMAGE_NOT_AUTHENTIC so my code is failing in SHCI_C2_BLE_Init()

I have a custom board with an STM32WB55CEU (512K Flash) that is failing to start the BLE stack on CPU2 in the function SHCI_C2_BLE_Init(). I believe it's failing this function because it failed to load the BLE firmware (stm32wb5x_BLE_Stack_full_fw v1...

0693W00000HobzdQAB.png 0693W00000HocOsQAJ.png 0693W00000Hoc2DQAR.png
DPars.2 by Associate III
  • 2853 Views
  • 5 replies
  • 0 kudos

Resolved! B-L072-LRWAN1: Why is the TCXO powered from PA12?

ie, what drove the choice of PA12, specifically ?Using PA12 means that you have to power-up the VDD_USB domain - which, I think, adds some extra current consumption. See:https://community.st.com/s/question/0D53W00001Fncm7SAB/stm32l072-vddusb-supply-c...

One-to-Many LoRa connection

Hi!Can someone help me to clear one moment in using LoRa.Let's say I have one RF remote control, which is pointed to 4-5 remote devices.How can my remote control distinguish replies from these 5 remote devices?Sorry if this is a dummy question. I'm n...

Zed by Associate III
  • 2883 Views
  • 3 replies
  • 0 kudos