STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Internal RTC Alarm Issues

We are currently developing two LoRaWAN-based products using STM32WL55J (battery powered and Mains AC). Both devices are designed to sample sensor data every 30 seconds and transmit it according to a defined daily duty cycle.However, we are facing ch...

STM32 Stop Mode 2 not entering

Hello everyone,I’m working on a project using the STM32WB55RG microcontroller with FreeRTOS, and I’m trying to put the MCU into STOP Mode 2. The system is supposed to wake up regularly using the RTC.I’m using LL libraries to configure the power regis...

STM32WBA65 in LDO scheme

Dear ST members,I'm designing a new board with STM32WBA65RGV6 in LDO power supply scheme. The datasheet and reference manuals are not clear how to connect certain pins in this configuration. Please, clarify the queries below:Is VDDSMPS to be connecte...

page-299.png page-302.png
rs-dp by Associate III
  • 367 Views
  • 1 replies
  • 0 kudos

CW RF signal WL55jc2 SUBGHZ

Hi,I'm trying to make continuous TX CW signal on 868.1 MHz or 432.4 MHz with the nucleo stm32 WL55jc2 without success. I spend a lot of times but sometimes goes wrong.I'm looking for somebody who as experienced with SUBGHZ and ping-pong as my app is ...

Franck95 by Associate
  • 350 Views
  • 0 replies
  • 0 kudos

Resolved! STM32WBA65RI usb device on stm32WBA65RI-DK1

Hello,I'm trying to implement a usb cdc device on a stm32WBA65RI-DK1 board but seems like the only usb otg supported is the usb st-link port  CN6 that supports USB_OTG_HS. Using cube mx, Im trying to configure that usb as device with the vbus enable,...

RPC by Associate III
  • 889 Views
  • 5 replies
  • 2 kudos

STM32WB5MMG cannot load userkey index 1 with SBSFU

Hello everyone,We are working on a project using a STM32WB5MMG, facing a strange situation with AES encryption userkeys. Our application code performs data encryption using the internal AES module and for that we load the (previously saved) internal ...

XaviF by Associate II
  • 367 Views
  • 1 replies
  • 0 kudos

Resolved! Persisting data in BKPSRAM with STM32WBA

Edited by a ST moderator to follow the community rules especially for code sharing. So please use </> to share your code   Hello, I am using the STM32WBA, and I am interested in persisting data to start after waking up from standby mode.I am unable t...

maborbaa by Associate II
  • 1680 Views
  • 11 replies
  • 0 kudos