STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! Pin sharing problem with SWD and SPI3, GPIO

Hi. I'm developing a custom board using STM32WB09TEF7TR microcontroller.I had a problem re-accessing the microcontroller using SWD once I finished programming one time.I found that it is due to the SPI3 (PA3) and one GPIO pin (PA2) sharing the pin fo...

KKIM.6 by Senior II
  • 1003 Views
  • 1 replies
  • 0 kudos

How to activate RTC calendar while using BLE.

 I want to send current date and time from mobile app(like nrf connect app) to STM32WB via BLE. Need to set that received time to RTC. From that time, RTC should update the date and time continuously. I don't know how to set that received time to RTC...

STM32WL55 module Low Power Problem

Hello,I am using the microcontroller STM32WL55Jc1 with the Nucleo WL55JC1 modules and I want to go into stop mode and consume as little as possible while ensuring wakeup via reception with LoRa signals. I have tried various configurations, but the me...

Henry77 by Associate II
  • 745 Views
  • 0 replies
  • 0 kudos

STM32WL55JC1 LoW Power Mode

Hello, I am using the STM32WL55JC1 microcontroller on the NUCLEO-WL55JC1 board and I tried the PWR_PLSLEEP example which is used to enter LPRUN mode. The example works, but the power consumption measurements are very different from those stated. In R...

Henry77 by Associate II
  • 1753 Views
  • 3 replies
  • 0 kudos

Blank WBA52 BLE Project Failing to Compile

Now that the BLE_wrap.c issue has been solved, I've gotten back to trying to develop my application for the WBA52KGU using STM32CubeIDE 1.17.0 and STM32Cube FW_WBA V1.5.0. Frustratingly, everything is still broken. Without the WPAN middleware enabled...

JLReyno by Associate II
  • 2448 Views
  • 5 replies
  • 1 kudos