NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
hello everyone, i am a beginner in STM32cube. i was working on board Nucleo wb55rg. and following this tutorial STM32WB Getting Started Series: Part 12a, STM32CubeMX & STM32CubeIDE lab. Introduction, and it said on 2:33 that i need to activate "syste...
HiIf I develop an application using the STM32WBA25 MCU with BLE, ThreadX, and USBX, is the RAM size sufficient?
Hello everyone!I am trying to get all services and characteristics from steval-stwinbx1 board running FP-SNS-Datalog2 function pack. Here's simple program I wrote:import asyncio from bleak import BleakClient MAC_ADDRESS = "DA:3E:83:DD:30:F8" async ...
Hi everyone, I am working on a Beacon project using NUCLEO-WB05KN. My goal is to broadcast Eddystone-UID and allow a connected phone to update the Namespace ID and Instance ID via GATT characteristics. The Setup: I have a Custom Service with two cha...
Hello, I'm using 2x NUCLEO-WB55RG boards with the unmodified BLE_MeshLightingPRFNode example from STM32CubeWB V1.24.0. Setup:- BLE Stack full v1.13.2.2 (stm32wb5x_BLE_Stack_full_fw.bin)- FUS v1.2.0- Provisioned with ST BLE Mesh app (tested on both iO...
Hello,I am working with STM32WB05KN in beacon mode (non-connectable advertising, legacy advertising).I am configuring advertising manually using:aci_gap_set_advertising_configuration()aci_gap_set_advertising_data_nwk()aci_gap_set_advertising_enable()...
I am using a STM32WB05KZ of a custom PDB, and I can not read a correct value of Vbattery.I have programed the ACD (+DMA) usgin CubeMX. I use DMA to read the analog inputs:ADC_Conv_Cplt = 0; HAL_ADC_Start_DMA(&hadc1, value, 3); uint32_t start = HAL_...
Hi, will ST extend I-CUBE-LRWAN support to include the new MuRata LBAA0QB1SJ-TEMP-EVK? Or offer a ST board based on LBAA0QB1SJ-295? Any suggestion on how to reconfigure the current I-CUBE-LRWAN version to work on the new EVK? We were previously using...
Hello, I've been trying to setup bi-directional communication with USB-HID on a custom board with STM32WB55CEU. I can send data to the PC from the STM just fine. My usb stack runs, enumerates and reports correctly. However, when trying to send Data f...
I am trying to develop a small scale lorawan app on a nucleo-wl55jc using the application example in stm32cube_fw_wl_v1.5.0 and have spent several hours trying to trace my error/bug in the software. All join attempts fail because the deveui as it app...