STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32L053R8T6 segment LCD

Posted on June 15, 2015 at 16:33Dear Forumers,Can you help me, how to control a 4x18 (com x seg; direck control) costum design LCD?I searched a lot, but i found mostly graphical LCD-s.Maybe an example?Thanks! #segment-lcd #the-stm32l0-series-embe...

arpad by Associate II
  • 2809 Views
  • 5 replies
  • 0 kudos

STM32F429 LTDC and SDRAM

Posted on June 16, 2015 at 14:26Is it possible to use internal RAM as a frame buffer for LTDC?Where exactly in std lib examples are external RAM and LTDC connected? It seems to me that the code is written on SDRAM address but I cannot find any DMA/D...

predrag10 by Associate II
  • 2931 Views
  • 6 replies
  • 0 kudos

stm32f429i-discovery dcmi->sdram address 0xD0000000

Posted on June 09, 2015 at 06:58Hello, I am working with stm32f429 using with a ov7670 camera with the dcmi using dma. It works fine if I do a capture into sram. I have also successfully initialized and tested the 8mb sdram @ 0xD0000000. What I wou...

prothan by Associate II
  • 1936 Views
  • 3 replies
  • 0 kudos

STM32F469 - Error in datasheet?

Posted on June 04, 2015 at 16:21Hello On page 18 of the http://www.st.com/st-web-ui/static/active/en/resource/technical/document/data_brief/DM00118914.pdfof the F469 MCU it is witten this about the DSI interface speed:Maximum speed per lane: 500Mbps...

Tantalum by Associate II
  • 1292 Views
  • 2 replies
  • 0 kudos

STM32F437 DCMI

Posted on May 07, 2015 at 17:43Hi ---I'm adapting working code from the STM32F407 Discovery platform to a custom board using the STM32F437. The process has been going well but I am having a problem with the DCMI. The control (I2C) channel works fine...

cmoses by Associate
  • 1174 Views
  • 2 replies
  • 0 kudos

SCCB emulation by I2C communication problem

Posted on May 13, 2015 at 01:17Hi,I have an application where I configure a OV7670 camera by SCCB bus (Omnivision thing) emulated by I2C...I used this sucessfully for couple of months but yesterday I disassembled the PCB that I have made for that ap...

Modal dialogs and pen up messages

Posted on April 13, 2015 at 23:39 I have a popup dialog that I load for some text entry. If I make it modal, the dialog procedure no longer gets 'pen up' events. If it is not modal, the user can interact with other things on the screen behind th...

hbarta2 by Associate III
  • 699 Views
  • 0 replies
  • 0 kudos

DCMI vs LTDC - simple Pinout on STM32F429 Discovery

Posted on March 31, 2015 at 20:32Hi! I have a simple yet hard problem. As is known, the STM32F429I discovery line has on board mainly ili9341 tft lcd. The job is to work with OV7670 camera through DCMI and with ili9341 through LTDC. But there is p...

sawingor by Associate II
  • 2727 Views
  • 5 replies
  • 0 kudos

STM32F417IGT6 FSMC A25 HardFault

Posted on April 12, 2015 at 11:16I have an ILI9325 TFT LCD connected to an F417IGT6 via FSMC Bank 1, Region 1, using 16-bits.The ILI9325 has an 8080-style interface, and FSMC A25 has been selected to drive register select as per AN2790 Figure 3 for ...

connect by Associate II
  • 2529 Views
  • 4 replies
  • 0 kudos