cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F469 - Error in datasheet?

Tantalum
Associate II
Posted on June 04, 2015 at 16:21

Hello

On page 18 of the

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/data_brief/DM00118914.pdf

of the F469 MCU it is witten this about the DSI interface speed:

Maximum speed per lane: 500Mbps1Gbps

Well, finally, is it 500Mbps or 1Gbps per lane? :D

Thanks

#stm32f469-dsi
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on June 04, 2015 at 17:12

Yes, looks odd, suspect it morphed from 1x lane 500 MBps, 2x lanes 1 GBps

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Amel NASRI
ST Employee
Posted on June 05, 2015 at 12:08

Hi Paul,

To precise: Maximum speed per lane is 500 Mbps. It will be fixed in the datasheet.

Thanks

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.