cancel
Showing results for 
Search instead for 
Did you mean: 

STemWin is stuck in GUI_Init() api on STM32F769IDISCOVERY board

AKonw
Associate

I am trying to get STemWin to work with mbed-os but it seems to be stuck in infinite loop inside GUI_Init() (can confirm the same over debugger).

I know for certain that the MCU is not stuck in hard fault since I have another thread running which is flashing an led.

Details:

I ams trying to run the basic hello world test (STemWin_HelloWorld) provided in STM32Cube_FW_F7_V1.14.0 with main thread writing to GUI and another thread flashing an led.

Snippet of code below:

main()

{

GUI_Init();

WM_MULTIBUF_Enable(1);

GUI_Clear();

GUI_SetFont(&GUI_Font32_1);

GUI_DispStringAt("Hello world!", (LCD_GetXSize()-100)/2, (LCD_GetYSize()-20)/2);

while(1) {

GUI_X_Delay(1000);

}

}

I have provided the necessary os apis for timing and multitasking in GUI_X_OS.c

I am linking the compiled object files to STemWin_CM7_OS_wc32_ARGB.a to create the MCU image.

I am calling the STM32 CRC hw module initialization api before calling GUI_Init().

The GUI memory assigned to STemWin library using GUI_ALLOC_AssignMemory() in GUIConf.c is word aligned.

Is there anything I am missing here?

Is the STemWin library (STemWin_CM7_OS_wc32_ARGB.a) tightly coupled to FreeRTOS?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0