Hello,As you have requested, I have ordered the board via ST e-store on March 1st. Also, I have got the order confirmation from ST.Further, when can I expect to receive the news of the seat reservation from ST ?Thank you and with my kind regards,Sue
Hello,I have been experiencing the following issue when working with CubeMX :#1. The EXECUTE button of the Graphics Middleware / STemWin Configuration panel does NOT open the GUI Builder, when it is clicked (activated). GUI Tool is enabled.Here is th...
Hello,I have been working on the graphics display on the STM32F429I-Disc1, but have been unsuccessful and facing errors so far.Here are my specifications :CubeMX 4.25.0IDE SW4STM32 from AC6Repository FW_F4 V1.23.0 Board STM32F429I-Disc1Purpose : crea...
Hello Sylvie and Tilen,I thank you for your great support to make the workshop works.So, my board functions properly as your requests on the homework : #1. The LD1 Green Led blinks.#2. Probes in and out are deployed via CubeMonitor.Look forward to se...
Hello again Sylvie,I am writing you this email to say that I worry about the board delivery from your ST direct supplier.So, as you have requested, I have ordered the board via ST e-store on March 1st.ST order number : ST36469My email address : supar...
Hello Sylvie,I thank you for your quick reply.If this may help, my order confirmation is ST36469 via ST e-store.My email address : supardi.sujito@epfl.chPlease feel free to contact me if you need more information.Have a nice day and with my kind rega...
Hi Wael,I thank you for your reply.Indeed, I use GUI Builder and STemWin to work with the graphics. So, I do not work with TouchGFX.I can not give you 100% positive reply on your question. However, my personal laptop does not produce this issues as m...
Hi Wael,I thank you for your reply.I have a close look on the files of my project, and I am not sure which file you would like to receive (name, type, extension). However, I have already enclosed an ioc file on my previous answer (my reply to Nawres)...