STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

I cannot get the Keil target to build without errors.

I am using the STM32F469I Disco board.I have created a project and then opened the generated Keil project. I simply try to build the generated project. The errors appear to be caused by not linking to the 'stm32f469xx.h' file. The correct compiler #d...

Matt3 by Associate II
  • 4173 Views
  • 4 replies
  • 0 kudos

Why does it say member function not declared.

Hi,I have been leaning how to use TouchGFX with the STM32F429I Discovery Board. I have managed to get buttons to work with hardware and for it to call Virtual function to toggle GPIO pins. however when i have tried to add a virtual function with a sl...

MikeP by Senior
  • 2356 Views
  • 9 replies
  • 0 kudos

Displaying JPEGs from extMemory not working

Hi,I'm currently trying to display a JPEG image in STemWin, which is loaded into extRAM. Therefore, I can use the GUI_JPEG_Draw() method, which (as the documentation states), should ALWAYS return 0. While it does indeed display the image and return 0...

Resolved! Missing variables textCounterBuffer and TEXTCOUNTER_SIZE

Dear, On https://touchgfx.zendesk.com/hc/en-us/articles/205443982 the variables textCounterBuffer and TEXTCOUNTER_SIZE are used in snprintf.  If I'm not mistaken, those variables are not available in TouchGFX 4.10.0. Is that correct?Thanks,Bart

BBoec by Associate II
  • 1571 Views
  • 2 replies
  • 0 kudos