STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX and UART Receive

Dear Sir,I am working in the R&D of Sectorqube. Our company has chosen the ST chip to be used for new product design and mass production. So presently I am using the 32F429IDISCOVERY board and a custom sized touchscreen of size 480 x 272. I am trying...

JKris.8 by Associate II
  • 10903 Views
  • 25 replies
  • 0 kudos

Assertion failed when using simulator ONLY from mvs

I'm working on a project on the STM32F746G-DISCO board, a colleague modified it to be used in kyle and succesfully be loaded on bord, and now when i launch the simulator via touchGFX designer, everything seems to works fine, but when i launch it from...

0690X000008iShlQAE.png
Zui by Senior
  • 1073 Views
  • 2 replies
  • 0 kudos

Resolved! TextAreaWildCard displaying too many characters

Hi,Imagine I have a vector of 10 different text Areas and I want to write a different number ranging from 0 to 9 on each of them (0 on the first one, 1 on the second and so on). What's the best strategy to achieve this? Using a wildcard definitely se...

GMeur by Senior II
  • 3217 Views
  • 11 replies
  • 0 kudos

Resolved! Enabling TouchGFX for STM32L4R9I-Disco board.

Hi, I setup CubeMX last version. I try to make a project for STM32L4R9I-Disco board. But in middleware section TouchGFX isn't seen. You can check from attached picture. How can I enable TouchGFX for this MCU.

Epamuk by Associate III
  • 2219 Views
  • 5 replies
  • 0 kudos

How to make a screen transition?

Hi, I want to make a screen transition by hardware button,i tried to make a screen transition by TouchGFX Designer Interactions and that works fine.But i have no idea how to make the same transition, using hardware button.I found an example like this...

qqAnton by Senior
  • 1251 Views
  • 1 replies
  • 0 kudos

TFT LCD and STM32f4 discovery

Hello, I am programming at Eclipse and i cannot get to work the ili9341 since i couldn't find the 8-bit parallel libraries. Do any of you have any examples?. I'm using the HAL libraries.Thanks.

EEscu by Associate
  • 1064 Views
  • 1 replies
  • 0 kudos