User Activity

Hi, my name is João.​I'm graduated in Electronics Engineering from Federal University of Santa Catarina and have more than 10 years of experience in electronics, working with hardware design, multilayers PCBs, firmware (bare-metal C/C++ and FreeRTOS ...
I'm using a STM32F7508-DK boar, so I need to run my code from QSPI flash. My application is running on target, but all the animations are slower than it should be. When running on simulator, everything runs perfect. Screen transitions without effects...
I'm building a new hardware based on STM32F7508-DK demo board. The display used by ST is the RK043FN48H-CT672B. According to Rocktech support, this display was customized for ST (with a single solderable flat cable). The touch and TFT driver ICs on t...
hi,I'm trying to follow the steps on "CubeIDE 1.0 and TouchGFX 4.10.0: Resolving integration issues" video and I still can't build a project from scratch on Cube IDE. I'm working with TouchGFX graphics too. Here is my build log:10:46:24 **** Incremen...
Kudos from