STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! No Support for svg Numbers in TouchGFX?

I am currently making an artificial horizon for a project in TouchGFX, but I just noticed that when I tried to use the svg of the Pitch_Angle_Indicator that has numbers I get a compile error. Are there any plans to implement the usage of numbers in s...

Neyus_0-1746559982988.png
Neyus by Associate III
  • 2972 Views
  • 8 replies
  • 2 kudos

Resolved! How to display image from QSPI flash?

Hi I've been trying to display an image on the GUI using an image (hex array) stored in the QSPI flash (memory mapped). I've taken a look at some of the documentation such as Loading Images at Runtime & Dynamic Bitmaps. void LandingView::loadImageFro...

Priyank by Senior
  • 1745 Views
  • 3 replies
  • 0 kudos

Resolved! how to initiate touchgfx slider event from code

Hi eveyone!I am using TouchGFX Designer 4.25.0In the real world, you can only move a linear slider control by touching/moving the slider knob itself. One of the issues with using the TouchGFX Slider Widget is that it will instantly move from one posi...

blueriver by Associate II
  • 2604 Views
  • 6 replies
  • 0 kudos

Questions regarding invalidate() and draw()

Hi!We got an old TouchGFX (4.10) application where the screen freezes from time to time. Freeze means we no longer get tick events, whereas the other FreeRTOS tasks are still alive. *Most* times this happens after Button pressed events.This raises un...

hvv by Associate
  • 1037 Views
  • 1 replies
  • 0 kudos

MVP base class moddified

Does anyone have an improved example to understand the MVP[1] (and widget/containers),where you change the base implementation of the MVP ?I was able to defined default implementation for the Model and the View but not for the Presenter or Drawables....

Marc_LM by Senior
  • 809 Views
  • 1 replies
  • 0 kudos

Resolved! How to execute/trigger an Interaction via code

I have a series of interactions that shows/hide widgets on the screen. The interactions are basically triggered when a button is clicked and are all managed via TouchGFX Designer.Is there a way to trigger them via code, so like generate a virtual cli...

nico23_0-1746003905602.png
nico23 by Senior III
  • 1454 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.