User Activity

Hello,I'm currently working on a project where I want to use both the NFC08A1 expansion kit and the RVA35HI display kit along with the U575ZI-Q development board. When I try to include the X-CUBE-TOUCHGFX software package in STM32CubeIDE, I get the f...
Hi there, I was trying to use the TouchGFX Designer Template for the H563ZI dev board with the RVA35HI display. However I noticed that I have REV1.0 of the display whereas the template that is generated is for REV1.1.I tried configuring the pin conne...
I've been trying to get the TouchGFX Project work for the above configuration. I have followed the following steps:1) Choose the demo project for the setup mentioned2) Generate code3) Open the project in STM32CubeIDE4) Build Project5) Add the generat...
Steps Taken So Far1. Downloaded the X-CUBE-NFC6 expansion pack on the STM32CubeIDE (Have already set up the project for my dev board)2. Configured the pins under platform settings for the expansion pack. I presume that this is where I have gone wrong...
Hi,I was trying to use TouchGFX for the RVA35HI display with the U575ZI-Q development board. In the product website it does say that there will be a demo project for the same. I am using TouchGFX Designer version 4.24.1 and am unable to find it.It wo...
Kudos from