User Activity

i have tried numerous time to add the file path for FatFS files in my project to makeFile, touch designer wont flash board because icant file the .Fatfs,h file.i was advised by ST employee to add file path to the MakeFile , not being a software engin...
when i try and flash the board through the designer it keeps failing. I have tried removing the files and creating a new folder and linking that one but no success, i am desperate my project is due to be presented on Friday, i have experimented with ...
i have use example from TouchGFX Demo 1, ive gone through code but cant see anything obvious. with the 746 Disco board, above.i set up the project through TouchGFX designer, only one screen and copied code from example, here is the view.cpp i have c...
Im using STM32F746 . i have the pixel format set the same in LTDC and TouchGFXgenerator, i have double checked the settings and recompiled the code several times, i wonder if i am missing something. any advice would be greatly received.thanking you i...