STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Selection best font for arabic texts

I have a problem, to present arabic texts on the screen.At the moment I use the font Janna LT Regular.Isolated letters seems not to be a problem. But if I want to write longer texts/words, then I see on the screen many "?"Is there an other font, whic...

MHase by Associate II
  • 5490 Views
  • 8 replies
  • 0 kudos

Resolved! Font Flash Section

Hi,I have ported the Application Template for NUCLEO-G071RB+X-NUCLEO-GFX01M1 to NUCLEO-F446RE+X-NUCLEO-GFX01M1.When i use external Flash for fonts, I do not see on the display all the text "relating to the language" (like "Use Joystick to Navigate" e...

ALomb by Senior
  • 1937 Views
  • 1 replies
  • 0 kudos

STM32L073 LCD Controller

I am trying to setup this LCD controller to drive a custom segment display, 22 segments, two backplanes.I have the code running, I can see the COM signals and can drive segments.I don't understand how the HAL LCD library works.from the HAL manual:HAL...

RSoen.1 by Associate III
  • 1151 Views
  • 0 replies
  • 0 kudos

Trivial question about customizing a keyboard

I redesign a layout of a keyboad (as I'm interested in numeric keys only, for a login).Everything is OK but I didn't managed to place the text of the key inside its button shape ( i.e. texts: "1", "2", etc appears outside the button)How can I tell wh...

Mvill.17 by Associate III
  • 1764 Views
  • 2 replies
  • 0 kudos

Using STM32CubeMX to setup LTDC: 1. If i resize the central area, when i visualize GPIO settings, it may happen that the vertical scroll bars are overloaded. It happens when the grid view width is bigger than the width of the hosting area

Multiple selection of rows are intended or it is a side effect?Why if i set the same functionality on the pin view of one pin it disables the LTDCGPIO Settings, the pin configuration area should be vertically resizable

FMarr.2 by Associate III
  • 772 Views
  • 0 replies
  • 0 kudos

Resolved! At TouchGfx documentation, chapter "TouchGfx on Low Cost Hardware", It's specified an SPI connection of 32MHz between STM32G0 uC and ILI9341V display controller. I cannot find in ILI9341V datasheet how to achieve that speed in SPI modes of the controller.

Datasheet specify a minimun serail clock for writing of 100ns. For sure I'm missing something because you have examples availables. Can you help in regards ?

IVill.1 by Associate II
  • 1707 Views
  • 4 replies
  • 0 kudos