Skip to main content
KKana.1
Visitor II
March 26, 2020
Question

TouchGFX 4.13.0 and STM32F469I Discovery kit (V3.0.0) IDE compilation errors for KEIL MDK V5.28 and SW4STM32 IDE. Needed some help.

  • March 26, 2020
  • 2 replies
  • 1161 views

Recently I started learning TouchGFX designer 4.13.0 with STM32F469I Discovery kit. I used getting started tutorial link. This is a amazing TFT designer tool. Simulation and target programming worked very well. STM32F469I-DISCO ioc file was generated as a default configuration. I used STM32CubeMX 5.6.0 for generating KEIL IDE and SW4STM32 projects.

However, compilation in SW4STM32 IDE caused an error listed below.

I searched for some fixes,  excluding from compilation simulation folder link

It didn’t resolve compilation error. Can you please explain the nature of error?

"../TouchGFX/target/generated/OSWrappers.cpp"

../TouchGFX/target/generated/OSWrappers.cpp:17:10: fatal error: touchgfx/hal/OSWrappers.hpp: No such file or directory

 #include <touchgfx/hal/OSWrappers.hpp>

         ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~

compilation terminated.

TouchGFX/target/generated/subdir.mk:27: recipe for target 'TouchGFX/target/generated/OSWrappers.o' failed

make: *** [TouchGFX/target/generated/OSWrappers.o] Error 1

KEIL MDK-ARM compilation errors

Build target 'STM32F469I-DISCO'

compiling TouchGFXHAL.cpp...

../TouchGFX/target/generated/TouchGFXGeneratedHAL.hpp(20): error: #5: cannot open source input file "touchgfx/hal/HAL.hpp": No such file or directory

 #include <touchgfx/hal/HAL.hpp>

../TouchGFX/target/TouchGFXHAL.cpp: 0 warnings, 1 error

compiling STM32TouchController.cpp...

../TouchGFX/target/STM32TouchController.hpp(23): error: #5: cannot open source input file "platform/driver/touch/TouchController.hpp": No such file or directory

 #include <platform/driver/touch/TouchController.hpp>

../TouchGFX/target/STM32TouchController.cpp: 0 warnings, 1 error

assembling startup_stm32f469xx.s...

compiling OSWrappers.cpp...

../TouchGFX/target/generated/OSWrappers.cpp(17): error: #5: cannot open source input file "touchgfx/hal/OSWrappers.hpp": No such file or directory

 #include <touchgfx/hal/OSWrappers.hpp>

../TouchGFX/target/generated/OSWrappers.cpp: 0 warnings, 1 error

compiling CortexMMCUInstrumentation.cpp...

../TouchGFX/target/CortexMMCUInstrumentation.hpp(4): error: #5: cannot open source input file "platform/core/MCUInstrumentation.hpp": No such file or directory

 #include <platform/core/MCUInstrumentation.hpp>

../TouchGFX/target/CortexMMCUInstrumentation.cpp: 0 warnings, 1 error

compiling TouchGFXConfiguration.cpp...

../TouchGFX/target/generated/TouchGFXConfiguration.cpp(17): error: #5: cannot open source input file "texts/TypedTextDatabase.hpp": No such file or directory

 #include <texts/TypedTextDatabase.hpp>

../TouchGFX/target/generated/TouchGFXConfiguration.cpp: 0 warnings, 1 error

compiling KeySampler.cpp...

../TouchGFX/target/KeySampler.hpp(42): error: #5: cannot open source input file "platform/driver/button/ButtonController.hpp": No such file or directory

 #include <platform/driver/button/ButtonController.hpp>

../TouchGFX/target/KeySampler.cpp: 0 warnings, 1 error

compiling TouchGFXGeneratedHAL.cpp...

../TouchGFX/target/generated/TouchGFXGeneratedHAL.hpp(20): error: #5: cannot open source input file "touchgfx/hal/HAL.hpp": No such file or directory

 #include <touchgfx/hal/HAL.hpp>

../TouchGFX/target/generated/TouchGFXGeneratedHAL.cpp: 0 warnings, 1 error

compiling TouchGFXGPIO.cpp...

../TouchGFX/target/TouchGFXGPIO.cpp(18): error: #5: cannot open source input file "touchgfx/hal/GPIO.hpp": No such file or directory

 #include <touchgfx/hal/GPIO.hpp>

../TouchGFX/target/TouchGFXGPIO.cpp: 0 warnings, 1 error

compiling Buttons.cpp...

../TouchGFX/target/Buttons.cpp(39): error: #5: cannot open source input file "touchgfx/hal/Buttons.hpp": No such file or directory

Can you please add in getting started section tutorials for other IDE's etc.

Best Regards,

Kamil

This topic has been closed for replies.

2 replies

Martin KJELDSEN
Principal III
March 31, 2020

Hi,

Glad you like the designer.

Your symptoms look like you haven't pressed "Generate code" from the designer, or your IDE isn't picking this up (Tried refreshing?). For Eclipse based IDEs we only rely on STCubeIDE from now on and don't do any testing in AC6, Atollic, Eclipse, etc.

/Martin

Giovanni Cambareri
Associate II
October 16, 2020

Hi,

I have the same issue:

16:33:25 **** Incremental Build of configuration Debug for project NUCLEOF746ZG ****

make -j8 all 

make: stat: ../Core/Startup/startup_stm32f746zgtx.s: Permission denied

arm-none-eabi-g++ "../TouchGFX/touchgfx/os/OSWrappers_cmsis.cpp" -mcpu=cortex-m7 -std=gnu++14 -g3 -DUSE_HAL_DRIVER -DSTM32F746xx -DDEBUG -c -I../Core/Inc -I../TouchGFX/touchgfx/framework/include/touchgfx/hal -I../TouchGFX/App -I../TouchGFX/target/generated -I../TouchGFX/target -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -I../Middlewares/Third_Party/FreeRTOS/Source/include -I../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -I../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1 -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-threadsafe-statics -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"TouchGFX/touchgfx/os/OSWrappers_cmsis.d" -MT"TouchGFX/touchgfx/os/OSWrappers_cmsis.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "TouchGFX/touchgfx/os/OSWrappers_cmsis.o"

arm-none-eabi-g++ "../TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterABGR2222.cpp" -mcpu=cortex-m7 -std=gnu++14 -g3 -DUSE_HAL_DRIVER -DSTM32F746xx -DDEBUG -c -I../Core/Inc -I../TouchGFX/touchgfx/framework/include/touchgfx/hal -I../TouchGFX/App -I../TouchGFX/target/generated -I../TouchGFX/target -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -I../Middlewares/Third_Party/FreeRTOS/Source/include -I../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -I../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1 -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-threadsafe-statics -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterABGR2222.d" -MT"TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterABGR2222.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterABGR2222.o"

arm-none-eabi-g++ "../TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterARGB2222.cpp" -mcpu=cortex-m7 -std=gnu++14 -g3 -DUSE_HAL_DRIVER -DSTM32F746xx -DDEBUG -c -I../Core/Inc -I../TouchGFX/touchgfx/framework/include/touchgfx/hal -I../TouchGFX/App -I../TouchGFX/target/generated -I../TouchGFX/target -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -I../Middlewares/Third_Party/FreeRTOS/Source/include -I../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -I../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1 -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-threadsafe-statics -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterARGB2222.d" -MT"TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterARGB2222.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterARGB2222.o"

arm-none-eabi-g++ "../TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterARGB8888.cpp" -mcpu=cortex-m7 -std=gnu++14 -g3 -DUSE_HAL_DRIVER -DSTM32F746xx -DDEBUG -c -I../Core/Inc -I../TouchGFX/touchgfx/framework/include/touchgfx/hal -I../TouchGFX/App -I../TouchGFX/target/generated -I../TouchGFX/target -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -I../Middlewares/Third_Party/FreeRTOS/Source/include -I../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -I../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1 -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-threadsafe-statics -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterARGB8888.d" -MT"TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterARGB8888.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterARGB8888.o"

arm-none-eabi-g++ "../TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterBGRA2222.cpp" -mcpu=cortex-m7 -std=gnu++14 -g3 -DUSE_HAL_DRIVER -DSTM32F746xx -DDEBUG -c -I../Core/Inc -I../TouchGFX/touchgfx/framework/include/touchgfx/hal -I../TouchGFX/App -I../TouchGFX/target/generated -I../TouchGFX/target -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -I../Middlewares/Third_Party/FreeRTOS/Source/include -I../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -I../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1 -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-threadsafe-statics -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterBGRA2222.d" -MT"TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterBGRA2222.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterBGRA2222.o"

arm-none-eabi-g++ "../TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterBW.cpp" -mcpu=cortex-m7 -std=gnu++14 -g3 -DUSE_HAL_DRIVER -DSTM32F746xx -DDEBUG -c -I../Core/Inc -I../TouchGFX/touchgfx/framework/include/touchgfx/hal -I../TouchGFX/App -I../TouchGFX/target/generated -I../TouchGFX/target -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -I../Middlewares/Third_Party/FreeRTOS/Source/include -I../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -I../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1 -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-threadsafe-statics -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterBW.d" -MT"TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterBW.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterBW.o"

arm-none-eabi-g++ "../TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterGRAY2.cpp" -mcpu=cortex-m7 -std=gnu++14 -g3 -DUSE_HAL_DRIVER -DSTM32F746xx -DDEBUG -c -I../Core/Inc -I../TouchGFX/touchgfx/framework/include/touchgfx/hal -I../TouchGFX/App -I../TouchGFX/target/generated -I../TouchGFX/target -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -I../Middlewares/Third_Party/FreeRTOS/Source/include -I../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -I../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1 -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-threadsafe-statics -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterGRAY2.d" -MT"TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterGRAY2.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterGRAY2.o"

arm-none-eabi-g++ "../TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterGRAY4.cpp" -mcpu=cortex-m7 -std=gnu++14 -g3 -DUSE_HAL_DRIVER -DSTM32F746xx -DDEBUG -c -I../Core/Inc -I../TouchGFX/touchgfx/framework/include/touchgfx/hal -I../TouchGFX/App -I../TouchGFX/target/generated -I../TouchGFX/target -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -I../Middlewares/Third_Party/FreeRTOS/Source/include -I../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -I../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1 -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-threadsafe-statics -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterGRAY4.d" -MT"TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterGRAY4.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "TouchGFX/touchgfx/framework/source/touchgfx/widgets/canvas/AbstractPainterGRAY4.o"

../TouchGFX/touchgfx/os/OSWrappers_cmsis.cpp:2:10: fatal error: touchgfx/hal/OSWrappers.hpp: No such file or directory

 #include <touchgfx/hal/OSWrappers.hpp>

     ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~

compilation terminated.

.....and other error lines

It seems that the IDE doesn't have access to the path where OSwrappers.hpp is included. (actually is included)