STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

How to Forward Data from TouchGFX?

In TouchGFX, data transfer is done as follows.Model.hppuint8_t TmpA;In Presenter.hpp,return Get_Data(){ return model-> TmpA;}Viwe.cppuint8_t Test;Test = presenter->Get_Data()I am doing the program in this way.But I heard that I shouldn't do this.When...

PKunK.1 by Associate III
  • 882 Views
  • 0 replies
  • 0 kudos

How to make a screenshot function with touchGFX?

Hello, anybody knows how to make a screenshot function with touchGFX4.12.3?Hardware: stm32f767+sdram,ltdc ,800*480 LCDI found a API STM32F7HAL::getTFTCurrentLine(), my logic is that when the current line is greater than 480, then __HAL_LTDC_DISABLE(&...

HWang.12 by Associate
  • 939 Views
  • 0 replies
  • 1 kudos

C++ standard used for TouchGFX generated code

Hello,I am wondering what C++ standard is used for the TouchGFX generated code?I checked in C:\TouchGFXProjects\ProjectName\gcc\Makefile but was only able to find -std=c99The concern is that if TouchGFX generated code with modern C++ (C++ 2011 and la...

RReta.1 by Associate III
  • 890 Views
  • 0 replies
  • 0 kudos

RGB controller interface and memory

hey,as i saw at the EVB, the driver uses the SDRAM as a memory source for the RGB interface.the SDRAM size is 256Mbit while the SRAM is 16Mbit.in my application, my plan is to use the SRAM only.Do you see any problem to use the SRAM memory for the RG...

Pkats.1 by Associate II
  • 1643 Views
  • 3 replies
  • 0 kudos

Resolved! touchgfx HardFault with STM32H743II

Hello,this is not the first time i set touchgfx in a custom board (with STM32F767 MCU). I always followed the method described in the touchfgx documentation, which can be summarized in this video guide.Now i'm trying to get it to work with STM32H743 ...

AMerc.4 by Senior
  • 2336 Views
  • 4 replies
  • 0 kudos

Resolved! How Setup a STemWin Project

Hello,i would like to start a project with a STM32H743, a 4 "TFTDisplay and STemWin. The sDisplay works perfectly via FSMC. Now I have downloaded the STM32Cube_FW_H7_V1.8.0. Which Lib should I use? In old versions they were marked with GCC. Now with ...