STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Importing Typographies

Hi,I want to use a TextLabel container found in another project.I manually edited the Designer's .touchgfx file and copied the relevant cpp/hpp files.Unfortunately, this class assume the presence of about 30 typographies and resources, which are of c...

CHech.1 by Associate III
  • 743 Views
  • 0 replies
  • 0 kudos

TouchGFX RGB Color Output Problem Questions.

Hello, I'm asking you this question because there is a problem that I couldn't solve during the Touch GFX test.First, let me tell you about the current environment.1. Evaluation board: NUCLEO-L4P5ZG2. IPS TFT-LCD 1) Resolution: 320 × 240, 16-bit colo...

0693W00000BbAcSQAV.jpg 0693W00000BbAahQAF.jpg 0693W00000BbAcwQAF.jpg 0693W00000BbAd6QAF.jpg
ybyeo.1 by Associate
  • 2923 Views
  • 4 replies
  • 0 kudos

Resolved! TouchGFX Colour issue

Hello,This is my first attempt on using the TouchGFX library, so I'm still learning how everything works. I've a custom board running on a STM32G473CBU6 with a 1.54" ST7789V LCD interfaced through SPI.I know the LCD driver is working because I can ru...

0693W00000Dn4SOQAZ.jpg
margce by Associate III
  • 3909 Views
  • 5 replies
  • 0 kudos

Resolved! Problems with ethernet and usb when using TouchGFX

HelloI'm working with a custom HW with a STM32H753 controller.The operating system is Keil RTX and Keil Middleware is used.I have a 272x480 display connected to LTDC (RGB565).I also have ethernet functionality implemented with a LAN8742A PHY and one ...

jimmii by Senior II
  • 3132 Views
  • 5 replies
  • 0 kudos

Resolved! Is it necessary to use RTOS for TouchGFX?

Hello,I'm using TouchGFX with STM32H757i-eval board I'm finding it difficult to configure for TouchGFX with RTOS.Is it mandatory to use RTOS while using TouchGFX.According to this link TouchGFX can be configured without RTOS.https://support.touchgfx....

Aarra.1 by Senior
  • 1735 Views
  • 4 replies
  • 0 kudos