2021-10-20 6:20 AM
Hi,
I want to use a TextLabel container found in another project.
I manually edited the Designer's .touchgfx file and copied the relevant cpp/hpp files.
Unfortunately, this class assume the presence of about 30 typographies and resources, which are of course tiresome to add manually, and therefore doesn't compile. (they show up in the TEXTS enum in TextKeysAndLanguages, for example).
I can't find which file to manually copy from the original project in order to add these typographies to my designer manually.
I have tried to copy the project's texs.xslx file, to no avail.
Any help would be appreciated!
Thank you