STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How to add TouchGFX 4.18 to STM32CudeIDE and MX?

Hi. I've followed the installation guidance found at https://support.touchgfx.com/docs/introduction/installation and can't get TouchGFX 4.18 to show up in neither STM32CudeIDE and STM32CudeMX (refreshed several times). Will this show up when an updat...

0693W00000FDV2TQAX.jpg
Mecanix by Senior
  • 4142 Views
  • 12 replies
  • 0 kudos

How the index are calculated from GUISetColor() for CLUT? Any configurations to be done for CLUT with emwin library

Hi,I'm trying to reduce the frame buffer size for LTDC, Therefore I'm using CLUTI configured for L8 pixel format and enabled the CLUT with input array of 256 size filled with color values.When I'm giving GUI_SetColor(Index_No); it is displaying rando...

MAnug.1 by Associate
  • 836 Views
  • 0 replies
  • 0 kudos

Resolved! HAL bug in glass LCD clock init (STM32L0)

in software package STM32L0 1.12.1in file stm32l0xx_hal_rcc_ex.cin functionHAL_StatusTypeDef HAL_RCCEx_PeriphCLKConfig(RCC_PeriphCLKInitTypeDef *PeriphClkInit)The RTC and LCD have their own settings, though they share the same clock.These settings a...

SZano by Associate III
  • 1436 Views
  • 1 replies
  • 1 kudos

Resolved! List of LCD drivers supported by TouchGFX ?

Hello,I want to know about the display drivers which touchgfx supported directly, so that I can decide which LCD suitable with TouchGFX like TouchGFX supports ILI9325 and OTM8009a.But I want to know complete lcd driver list.Thanks in advance.

R. by Associate II
  • 11645 Views
  • 19 replies
  • 0 kudos

How to use the LCD in the f429i discovery board with CubeIDE? In the old cubemx examples there are rich libraries to draw, write, etc on LCD, but they're not updated to the CubeIDE Hal drivers.

You can import demo projects from the Cube package downloaded by the IDE, but you cannot integrate the libraries in a CubeIDE project, because they use different drivers. All you're left with in the new IDE is low-level functions. Is there a software...

MAles.1 by Associate II
  • 4693 Views
  • 9 replies
  • 0 kudos

Change Drawable text

Have ListLayout to which MenuItemToggle items have been "add".I believe ListLayout can be traversed via getFirstChild and getNextSibling.How to update menu item text?I presume the Drawable object returned by getFirstChild or getNextSibling can be use...

Weird Multiple Keyboard Issue

I am unable to add two Keyboards at the same time to the screen. One is alphanumeric and other is numeric only. The Keyboards work separately if the included header file is commented.#ifndef SCREEN_DIALOGVIEW_HPP #define SCREEN_DIALOGVIEW_HPP   #incl...

BKazi.1 by Associate II
  • 1190 Views
  • 1 replies
  • 0 kudos

LCD Freezes after running for a long time

I am using TFT LCD + LTDC + STemWin in STM32F429IG with external SDRAM. I have enabled multi buffering to reduce the flickering effect. Then it works fine. But after a continuous run time of more than a day the system is running al the freertos task ...

S_1 by Associate III
  • 2581 Views
  • 4 replies
  • 0 kudos