STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Question about LCD-TFT controller

I am new to STM32H7xx, and in the datasheet of these microcontrollers I read:"...The LCD-TFT display controller provides a 24-bit parallel digital RGB (Red, Green, Blue) and delivers all signals to interface directly to a broad range of LCD and TFT p...

imarz.1 by Associate III
  • 1367 Views
  • 1 replies
  • 0 kudos

[TouchGFX] Reusable Modal window on every screen?

Hi everyone,I'm currently working on a project where the device has to continuously read files from USB but where a user can also plug the device into a computer and mount it as a USB device to transfer and delete files and what-not. Now, I can detec...

Resolved! How to get list layout click value

I can use listLayout add() item and remove() item good, but I don't knowhow to get selected item number on callBackHandler()?Have any example for me to study ?​void Screen2View::callBackHandler(CustomContainer2 & cc_1){​ listLayout1.remove(cc_1); inv...

YCF.1 by Associate III
  • 3312 Views
  • 3 replies
  • 0 kudos

TouchGFX how to get the type of my Drawable

Hi,I have multiple Drawable on my screen and I want to change the color. I decide to iterate through my screen and depending of my drawable perform some modification. Right now I am using typeid() to extract the Drawable, it work for some Drawable bu...

aabba.1 by Associate III
  • 1573 Views
  • 2 replies
  • 0 kudos

TouchGFX Problem with HAL_Delay in while Loop

Hi, I've started a project STM32CubeMX and CubeIDE. I initialized a 4.3" TFT with LTDC and TouchGFX without RTOS. The function MX_TouchGFX_Process is in main while loop. At first everything were OK and my screens were updating very well. But for some...

Karim by Associate II
  • 880 Views
  • 0 replies
  • 0 kudos

Resolved! Header files STM32WB conflict with TouchGFX

I try add to pnucleo WB55 project touchgfx package and result is../Drivers/CMSIS/Device/ST/STM32WBxx/Include/stm32wb55xx.h:1084:29: error: expected identifier before '(' token 1084 | #define LCD ((LCD_TypeDef *) LCD_BASE) | ...

MM..1 by Chief III
  • 1847 Views
  • 2 replies
  • 0 kudos

Resolved! How to avoid creating too many similar widgets

I am makeing a gauge background out of many circle widgets. I dont want to use static immage background because the position of segments can change depending on the maximum rpm. I have create this in TouchGFX designer and for each circle widget Desig...

0693W00000LyK1mQAF.png
manto.1 by Senior
  • 1415 Views
  • 1 replies
  • 1 kudos

Begin frame and End Frame Process

Hi everyone,I want to learn something about "Begin Frame" - "End Frame" process. If touchgfx "Begin Frame" has started, will it come to "End Frame" status no matter what happen. For example code status is "Begin Frame" but something is changed (scr...

Epamuk by Associate III
  • 1521 Views
  • 1 replies
  • 0 kudos