STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX Designer to STM32IDE

Hello,basically I've got myself STM32WB55 evaluation board and NUCLEO-GFX01M2 display module, to test out the TouchGFX Designer.And right at the start I got a problem I can not solve myself. After I've created a simple project in Designer and flashed...

wingding 3 font does it work with touchGFX

Hi,I am trying to use wingding 3 font...In the touchGFX Designer I can see the character (arrow...) but when running the simulator there is no text area. -Any idea how to solve this issue? - Can we design a special character on touchGFX?Thank you

aabba.1 by Associate III
  • 1309 Views
  • 2 replies
  • 0 kudos

Resolved! TouchGFX - Truncated line when using word wrapping

Hello,I'm working on a TouchGFX GUI and I have some text areas which need to be automatically wrapped on several lines.I'm using Text_guideline.setTypedText(touchgfx::TypedText(guideline)); Text_guideline.setWideTextAction(WIDE_TEXT_WORDWRAP); Text_g...

0693W00000LvlAfQAJ.png 0693W00000LvlAVQAZ.png
Aksl by Associate III
  • 4048 Views
  • 9 replies
  • 0 kudos

How to re-create a missing .ioc file?

I'm running the LTDC_Paint example for a STM32F429i_DISC1 board on CubeIDE. The files in the package do not comprise the .ioc file that could allow to change the uC configuration. Is there a way to re-create this missing file?Thanks for your help!

Dlinky by Associate II
  • 1983 Views
  • 3 replies
  • 0 kudos

Question: Dynamic Bitmap Cache and Memory Used

Hello all,​ I create a custom container in TouchGfxDesigner and I want to used Dynamic Bitmap Cache and Memory:​class Knob : public KnobBase{public:  Knob()  {    Bitmap::cache(BITMAP_ENTER_1_ID);    Bitmap::cache(BITMAP_ENTER_2_ID);    pbuf = new u...

V.H by Senior
  • 1136 Views
  • 1 replies
  • 0 kudos

Remote Access over WiFi?

I would be interested in making the TouchGFX GUI for my device accessible over WiFi. What I would like to do is type a URL, and reach a page to operate and configure my embedded device. Is this possible?

SShah.22 by Associate
  • 2204 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.