STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX app store functionality

Hi,I'm looking at how compiling TouchGFX applications work, and it appears that you have to compile the TouchGFX project and then flash the board with the application.https://support.touchgfx.com/4.19/docs/development/ui-development/working-with-touc...

DOkaz.1 by Associate II
  • 1333 Views
  • 2 replies
  • 0 kudos

Scrollable Container in design mode

Hi , Please help me! How can I to scroll in design time in a scrollable container? I want to create an interface, what is have more info than can fit on the screen. That’s why I want to scroll , because that's it very complicated to do the design. Is...

0693W00000Nrx0cQAB.png
KGulacsi by Associate
  • 972 Views
  • 1 replies
  • 0 kudos

Issue With ST new Cube , TouchGFX

CubeMX 6.5.0, Cube-AZRTOS-H7 V2.1.0, TouchGFX 4.19.1make a new project , using threadX os, gui using TouchGFX, project error.MX_TouchGFX_Init(), need input VOID *memory_ptr, but empty.do not excute MX_TouchGFX_PreOSInit();do not excute OSWrappers::i...

Breeze1 by Associate III
  • 1116 Views
  • 1 replies
  • 0 kudos