STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX font distorted

I have TouchGFX UI running on STM32H7. Only with one screen there is an issue, fonts gets distorted.   What could be the reason for this?  

VNA_0-1754397210983.png VNA_2-1754397269439.png
VNA by Associate II
  • 1249 Views
  • 8 replies
  • 0 kudos

Resolved! Convert wstring to Unicode String

I have a multi-language graphics project which requires the use of characters beyond the standard ASCII set.  I have not found a working method to convert C++ wstring to TouchGFX::Unicode.  I have attempted the following: Unicode::strncpy(txtTitleBuf...

RLarr.1 by Associate III
  • 818 Views
  • 4 replies
  • 3 kudos

Resolved! Issues with SVG image rendering

Hi,I have a project derived from the demo6 from ST on the STM32U5G9J-DK1 devkit, where I want to display SVG images. The only difference is that the rounded display of the original kit has been substituted with another rounded display of the same res...

apadom by Associate III
  • 5156 Views
  • 35 replies
  • 13 kudos

Resolved! Changing TouchGFX TextArea font at runtime

I want to change the font at runtime for a TextAreaWithOneWildcard.I figured it would be as simple as:1. update the text in the wildcard buffer (previously set by calling setWildcardTextArea)2. call setTypedText( id ) where 'id' is a designer defined...

dave2012 by Associate III
  • 706 Views
  • 3 replies
  • 1 kudos

Transition Screen abnormal

Hello,I am a beginner with TouchGFX. I created two screens with a slide transition and found some questions would like to confirm.1) Text brokenI found that when the B screen transitions to the A screen, the Big Text contains text broken during trans...

TesterSAM_1-1760517705545.png TesterSAM_3-1760518548270.png TesterSAM_2-1760518117488.png TesterSAM_4-1760519008393.png
TesterSAM by Associate III
  • 509 Views
  • 2 replies
  • 0 kudos

How to use DSI_TE_DSILINK?

My project is working as expected using the DSI_TE_EXTERNAL with a TE pin from the display.How to get the TE event via DSI? Is that default enabled?If I use "CmdCfg.AutomaticRefresh = DSI_AR_ENABLE;" then I get the interrupt to my callback. But timin...

KRasm.2 by Associate II
  • 996 Views
  • 2 replies
  • 0 kudos