STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX update widget data from main() non-RTOS

I've created a TouchGFX project for an LTDC LCD with a H7a3 Nucleo board.  The project includes a static graph displayed on the LCD.  The project will compile, run and properly display the TouchGFX designed screen with the static graph. Next step wou...

SJR1 by Associate II
  • 2955 Views
  • 3 replies
  • 1 kudos

Resolved! Touch gfx code optimization

hello, I'm currently developing an application that features more than 150 screens. However, I've encountered a significant challenge: once I build the code, the overall size exceeds the available flash memory. While I'm using external flash for imag...

Not able to use touchGFX on Linux

Hi, i am using linux and want to customise STM32U5A9 discovery kit display. I am not able to use touchGFX in Linux. Also if i create a project in windows for touch GFX and try to build in it Linux stm32cubeide i am getting  TouchGFX/target/CortexMMCU...

Unknown2 by Associate
  • 762 Views
  • 0 replies
  • 0 kudos

No ST-Link detected after disconnect

 Hello ST Community,I’ve been working on a project to enable TouchGFX on my STM32H735-DK, but instead of using the TouchGFX Designer, I decided to configure everything manually to display a pre-designed image on the screen.The IssueInitially, everyth...

HispaEmo by Associate III
  • 1897 Views
  • 4 replies
  • 1 kudos