Skip to main content
Associate II
August 30, 2024
Solved

Lots of errors when building basic project

  • August 30, 2024
  • 7 replies
  • 2642 views

I have a CubeIDE project for a H743IITx board and an LCD and I added Touchgfx. The Touchgfx 4.24 contains the typical demo that switches between two screens. It runs fine in the simulator. I refreshed the project and it added all the necessary folders/files. Touchgfx is installed on the PC and the package was added inside the CubeIDE manager.

As you can see in the screenshot, there are a lot of red underlined files when I attempt to build the project. There are about 240 errors.

Usually, when so much code is underlined, it's a matter of missing libraries due to some kind of incomplete setup. However, I don't know what is wrong. I followed the documentation setup as well as different videos on youtube and actually the initial setup is not that complex.

Any ideas what could be missing?

 

This topic has been closed for replies.
Best answer by aro

I realize that the project I created in Touchgfx is a Simulator project for Windows. Maybe that's why all those errors in CubeIDE.

7 replies

ST Technical Moderator
August 30, 2024

Hello @aro ,

Probably, the Include paths are not properly set up and you are missing the include files.

You have to review the defines and project's Include path.

You can also start your project from STM32CubeMX and follow this tutorial.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
aroAuthor
Associate II
August 30, 2024

Yes, that's the document I used. The project built perfectly fine without Touchgfx. The problem started after I added it. In the screenshot, I think all paths are included.

GaetanGodart
ST Employee
September 2, 2024

Hello @aro ,

 

To summarize :

  • you created a project using STM32CubeIDE, it worked fine
  • you added the x-cube-touchgfx middleware, did it work fine there without changing the project?
  • you opened TouchGFX Designer and made a simple design, it worked in simulator
  • you refresh the STM32CubeIDE project, you now have underlined files and folders and it doesn't compile

Is it the first time you work with TouchGFX?

Can you share the errors? We can have a quick look through it to see if they say files are missing or something else.

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
aroAuthor
Associate II
September 2, 2024

Your bullet points are correct. It's the first time I'm using Touchgfx. I attached the console output.

GaetanGodart
ST Employee
September 3, 2024

Hello @aro ,

 

The build log's error are of type "undefined reference to "touchgfx::Font::getMaxTextHeight(unsigned short const*, ...) const".
So you have a lot of undefined references to functions which indicates that you are missing some includes, some path or similar.

I will assume that something is not included.

To try to fix undefined functions you can try multiple things:

  1. clean and rebuild the project in STM32CubeIDE (maybe all the changes were not taken into consideration)
  2. check the include files (check it for c and c++)
  3. check the linker settings (make sure it includes TouchGFX library, that is a .a file)

Furthermore, you can check where those functions are located with software able to do advanced searches (ex : Everything) and then double check that the file where it is defined/declared is available to your project.

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
aroAuthorBest answer
Associate II
September 4, 2024

I realize that the project I created in Touchgfx is a Simulator project for Windows. Maybe that's why all those errors in CubeIDE.

GaetanGodart
ST Employee
September 4, 2024

No problem @aro , it happens to the best of us! ;)

The best way to learn how to follow our documentation : board-introduction 

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)