STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Generating LL library for FDCAN

Hi Team,I am working on SIL2/3 compliance project. For this I need to generate and work on LL based libraries instead of HAL libraries.I am using STM32Cube v1.19.0. and working on STM32H753xx and STM32G4A1VET6 series MCU.I am unable to generate LL li...

Abey by Associate
  • 118 Views
  • 6 replies
  • 2 kudos

Creating HID keyboard using USBX

I'm trying to generate an HID keyboard through CubeMX for USBX. I'm using an F411CE based board so picked the appropriate software pack for that. However, when I go to pick to pick components, I can only see the generic HID pack instead of separate k...

How to transfer usb cdc data using DMA?

Hello everyone.I am using st32f407 chip to drive ad7606c ADC chip, and I want to output real time graph from PC to matlab via usb.ad7606c outputs busy signal at the end of conversion, and GPIO callback function is executed like below according to bus...

ildong by Visitor
  • 56 Views
  • 1 replies
  • 0 kudos

STM32H7 + LAN8742: No DHCP Request Observed

Hi,I'm using an STM32H7 board with a LAN8742 PHY, configured via STM32CubeMX.LwIP is initialized without RTOS, and Ethernet is in RMII mode.The main goal of this project is to receive data over UART and forward it via Ethernet.I want the STM32 board ...

WhatsApp Image 2025-07-14 at 16.08.30_914e31a7.jpg WhatsApp Image 2025-07-14 at 16.08.30_c81398da.jpg
Matan by Visitor
  • 29 Views
  • 0 replies
  • 0 kudos