STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1746 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4898 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9605 Views
  • 5 replies
  • 3 kudos

Issue in running motor using custom board STSPIN32F0

Dear, I have custom board based on this https://github.com/issus/BLDC-Drive which uses STSPIN32F0 as motor driver. I have that got that PCB manufactured & assembled but stumbled on an issue (which I assume is an issue) that it does not have feedback ...

x4ce by Associate III
  • 1777 Views
  • 2 replies
  • 0 kudos

B-G431B-ESC1 with FOC

I am trying to run an A2212 13T motor with B-G431B-ESC1 motor with FOC algorithm.But the motor gets stopped after attaining a low speed.Solve the problem.

Resolved! Custom Board bringup issues

[VERSION]: 6.3.1[TOOL]: Board Designer, Motor Pilot, MCSDK[DETAILS]: Created custom board based on IHM16M dev kit, using STM32G431RB + DRV8323. Motor Pilot cannot spin motor, but encoder signals look accurate, Vbus signal is accurate, and current sen...

shanemattner_0-1731091672956.png shanemattner_1-1731091696880.png shanemattner_2-1731091711399.png

Resolved! MC Workbench6: Import a new motor

Dear all,Background: I am in a student project trying to build a robot for RoboCUP - SSL. We have elected to go with DF45L035048-A from Nanotec. I have not received the motors but I saw that it is possible to import a new motor with a .json file. I k...

Stickkan by Associate II
  • 2388 Views
  • 4 replies
  • 2 kudos

B-G431B-ESC1 6-step algorithm

I have an A2212 13T motor with B-G431B-ESC1 with  6-step trapezoidal algorithm.It is tracking the speed reference input.But the problem is that it takes time to reach the desired speed.Suppose currently my motor speed is at 5000 rpm, but if I change ...

Resolved! PFC in MCSDK-6.3.2

Hi, I recently tried SDK 6.3.0, 6.3.1, and 6.3.2. The Board Designer tool is the best for me. It's pretty cool and nice. With this tool, I can easily design the board for motor control. However, I would like to know the reason for adding the feature ...

Agga by Associate II
  • 1153 Views
  • 1 replies
  • 0 kudos