cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX Project breakdown

Sergiu_Pascari
Associate

Hello everyone, I ran into a problem when re-generating a project in a СubeMX.
If I make some updates in the peripheral settings and generate a project in the mx cube, my build goes through without errors and warnings. But if I load this project into the microcontroller, it refuses to work and even debug does not work, I assume that it is a hardware fault.
I use the latest versions of software
With first generation and loading everything works fine, but with repeated generation the project breaks.
How can I solve this problem? I’m tired of creating new projects every time.

The microcontroller is completely inoperative; communication through the motor; the pilot does not work as can be seen in the picture.
and when debugging, if I click Resume, the debugging turns off

Sergiu_Pascari_0-1715682803583.png

Sergiu_Pascari_1-1715682865499.png

 

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0