STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1763 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4915 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9643 Views
  • 5 replies
  • 3 kudos

Resolved! How to set the value of hFinaltorque?

Hello Everybody,MCSDK:6.3.0CubeMX: 6.3.0Workbench : 6.3.0Motor Pilot : 1.2.9Power Board : IHM08M1(Rshunt=0.01Ω)Control Board : NUCLEO-G431RBMotor : BLDC 26w 24v/8 pole pairs / rpm=4k / rated current=1.8A/hall sensorI am currently testing torque contr...

Vincent7 by Associate III
  • 7720 Views
  • 11 replies
  • 2 kudos

BLDC motor Control

Myself using STM32 G474RE board , please someone help me with step by step process with BLDC motor six step commutation control with code."I want to control BLDC motor in six step method using STM32G474RE (nucleo board)".Thank You !@Kenji1 

ses by Associate
  • 2044 Views
  • 1 replies
  • 0 kudos

A question about 6-step for X-NUCLEO-IHM16M1

MC Workbench generates a 6 step_sensless code for the following board: Type: 6-Step / Voltage Mode Control: NUCLEO-G431RB Power: X-NUCLEO-IHM16M1Motor: GimBal GBM2804H-100T Code: pwmc-3pwm.c in middle-ware       Question: In each step, it looks like ...

Motor speed uncontrollable

I am using STEVAL-ESC001v1 and a2212/10t 1400kv motor. While giving it supply and reference signal, the measured speed keep on increasing and the actual speed of motor as well. Also, motor_state stucked at START but motor still running. Please help. 

Field Weakening not working in ESC

I am using STEVAL ESC 001V1 and enabled Field weakening with FOC, but motor is not running, it is starting, stopped, starting stopped and soon. I also seperately tried setting Id = -ve value but its not working. Please help.

MCSDK documentation and your feedback

Motor Control Wiki: STM32 Motor Control Knowledge Database - stm32mcuMC Frequently asked questions (FAQ) for version MCSDK5.x:Frequently asked questions (FAQ) - stm32mcu   The documentation of the Board descriptions format is now available on the Mot...

Zied b. by ST Employee
  • 8338 Views
  • 2 replies
  • 9 kudos

Resolved! STSPIN32G4 PWM Output Jitter

Created a new thread from STDRIVE101 PWM Output Jitter Inquiry here because it is a question about a completely different device.Dear Peter,Thank you for your explanation. That clarifies the behavior of the STDRIVE101.I have two follow-up questions:D...

ajietb by Associate II
  • 2444 Views
  • 4 replies
  • 0 kudos

Resolved! SVPWM and BEMF Wareform type

Hello Everybody,MCSDK:6.3.0CubeMX: 6.3.0Workbench : 6.3.0Motor Pilot : 1.2.9Power Board : IHM08M1Control Board : NUCLEO-G431RBMotor : GBM2804H-100TI am currently testing FOC-OpenLoop-Voltage. I am using Motor Pilot for tuning and measuring SVPWM (at ...

Vincent7 by Associate III
  • 2418 Views
  • 5 replies
  • 1 kudos