STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1731 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4879 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9575 Views
  • 5 replies
  • 3 kudos

MCSDK_v5.2.0 availability

Hello Everyone,We are working on a motor control, inverter drive strategy demonstrator unit using an STM32 MB1136 C-04 board.To start, we have a legacy example program for motor control, for which I could get the properly old CubeMX version, bit it a...

fszabi01 by Associate
  • 813 Views
  • 1 replies
  • 0 kudos

While Running Motor Starts Jerking.

Dear Experts,I need your help to figure out a problem in my MC configuration. I am using Nucleo-F401RE and a custom motor Driver board similar to STEVAL-IPM20B with 0.01R shunt resistor and opamp used it LM324. The current sense circuit in my custom ...

Screenshot from 2025-02-06 18-45-34.png Screenshot from 2025-02-06 18-45-42.png Screenshot from 2025-02-06 18-45-27.png Screenshot from 2025-02-06 18-45-49.png

Custom STSPIN32 Board flashing not working

Hello STM Community,We are developing a custom motor driver board based on the STSPIN32F0251 and are encountering challenges with consistently flashing firmware onto the device. Below, I’ve shared our schematic (STSPIN schematic on page 3) and the st...

kenni by Associate II
  • 1186 Views
  • 0 replies
  • 0 kudos

Resolved! MC Workbench 6.3.2 B-G431B-ESC1

Hi everyone,I'm working with the B-G431B-ESC1 board and need help setting up overcurrent protection. I want to ensure safe operation and prevent damage to the hardware.Could anyone guide me on the best way to configure the current sensing and protect...

LSerhii_0-1738769957414.png LSerhii_1-1738770007818.png
LSerhii by Associate
  • 1834 Views
  • 2 replies
  • 0 kudos

Unable to do Pin mapping in MCSDK 6.3.2!!!!

Hi Everyone,Currently I am stuck at place where I want to do some changes in default assigned pin of motor SDK 6.3.2 but unable to do after Version 6.I was able to do it in MCSDK 5.x.x.. Versions.if you have any idea about changing pin mapping of ADC...

Akkii by Associate
  • 959 Views
  • 2 replies
  • 0 kudos