2024-07-17 10:08 PM
[This inquiry was made using a translator. Please understand.]
hello.
I would like to inquire about how to control a BLDC motor using the L6229Q motor driver.
The operating environment is as follows.
MCU: STM32G431KBUx
MotorDriver: L62229Q
The motor was controlled using the PWM of the MCU.
The PWM signal is connected to the Vref pin of L6229Q.
PWM frequency: 16.6kHz
The motor works well, but there are two problems.
The schematic of L6229Q is attached.
If you know the cause, please help.
2024-07-18 12:11 AM
In case of problem number 2, it does not seem to be a circuit problem as the sound comes from the motor rather than the PCB.