STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1716 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9546 Views
  • 5 replies
  • 3 kudos

Resolved! Issues build simulink project with CRL "ARM CMSIS SIN COS" and SW4STM32. Error: unknown type name ‘__IO’

Hello, i have a problem to build in PIL mode PMSM_FOC example. The problem is in the use of CRL: "ARM CMSIS SIN CON". After has manually add of the arm_math.h directory (C:\MATLAB\STM32-MAT\STM32\CRL\CMSIS_SIN_COS_CRL\FastMathFunctions) in the includ...

Resolved! How to make an automatic reset of the stepper motor pulse in STM32F407 without need to put it low manually?

Hi everybody,I'm working on 10 stepper motors controller using STM32F407vgt6. Is there any way how to automatically turn off the step pulse after I turn it on programatically? Maybe something with timer(s)? Some turn off delay? The pulse should be tu...

Branio by Associate
  • 2093 Views
  • 2 replies
  • 0 kudos

Resolved! Steval - spin3204 and motor jk86bls71-03-x001

Hello. I am using Steval - spin3204 and motor jk86bls71-03-x001. I am building a project for Keil in ST Motor control 5.4.3. But I can’t start the engine with or without Hall sensors. I tried to make various configurations of PID controllers, PWM par...

DTrif.1 by Associate
  • 1392 Views
  • 1 replies
  • 0 kudos

Resolved! how to drive P-NUCLEO-IHM001?

product link is here https://www.st.com/en/evaluation-tools/p-nucleo-ihm001.html. The purpose is to control the motor to run as requested, in the product page, I'm a little confused, I start the board f302r8 and start a project, then where to get the...

adam.wu by Associate II
  • 1320 Views
  • 1 replies
  • 0 kudos

Resolved! FOC Software for Nucleo-64 G474RE

Hi,I have recently bought an STM32 Nucleo-64 G474RE. I want to use this MCU for FOC with a BLDC. I have seen there are many libraries available and there is the ST Motor Control Workbench tool available. But I am confused as to which tool and/or lib...

CBald.1 by Associate II
  • 1348 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 Nucleo-64 G474RE board - FOC Software

Hi,I have recently bought an STM32 Nucleo-64 G474RE. I want to use this MCU for FOC with a BLDC. I have seen there are many libraries available and there is the ST Motor Control Workbench tool available. But I am confused as to which tool and/or libr...

CBald.1 by Associate II
  • 1191 Views
  • 1 replies
  • 0 kudos

Resolved! Is MC Workbench compatible with NUCLEO-64 G474RE ?

Hi,I am trying to use the MC workbench with a Nucleo-64 G474RE MCU. I have checked the boards in the software but mine does not appear. Is there any way I could use the Workbench with my Nucleo-64 G474RE MCU ? Any board form the ones listed which is ...

CBald.1 by Associate II
  • 1271 Views
  • 1 replies
  • 0 kudos