STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9546 Views
  • 5 replies
  • 3 kudos

Resolved! I'm using the STM32 Motor Control Software Development Kit (MCSDK) and every time I try to compile a project a get this error: "Temporary JSON file is corrupted ". Does anyone have experience solving this?

ERROR:Temporary JSON file is corrupted => switch to non-temporary and retryorg.json.JSONException: A JSONObject text must begin with '{' at 1 [character 2 line 1]Version info: MC Workbench    : 5.4.3.19514WB_to_Mx      : 1.0.6.template-19-11-14STM32C...

SQuin.1 by Associate
  • 1342 Views
  • 1 replies
  • 0 kudos

Resolved! what is the voltage range for X-NUCLEO-IHM03A1?

According to product page X-NUCLEO-IHM03A, this motor driver voltage range should be between 10.5 V to 85 V. But I got a sample I do see Vin max printed as '50V'. Can someone from the nucleo explain which max voltage spec I should choose?

轩郭.1 by Associate
  • 1228 Views
  • 1 replies
  • 0 kudos

Resolved! hi everyone ! need some help with STM32F401RE i m gana read 6 analog input using ADC with DMA and timer then i wana call the values from the memory to use it in the same time i wana made PWM output for my servo motor .

 I solved ADC and DMA part but i have problem whit calling the the values from memory and with PWM output that my servo motor cant work any way . plz help me:smiling_face_with_smiling_eyes: .NOT: im new in stm32

Halra.1 by Associate II
  • 5104 Views
  • 12 replies
  • 0 kudos
TB by Associate III
  • 2157 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F FOC SDK User Manual

Is there a newer version for the DocID18458? UM1052 is a very nice (but outdated) user manual for the FOC SDK for STM32F microcontrollers, it is more complete than UM2374 but has not been updated, or at least I can not find a newer version, since Sep...

kswarm by Associate II
  • 2768 Views
  • 1 replies
  • 0 kudos