STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1716 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9546 Views
  • 5 replies
  • 3 kudos

Resolved! SiC inverter design - high switching frequency

I am designing a SiC inverter for a Formula SAE student team, using a 72MHz STM32F302CC with the motor control library. The desired switching frequency is 50-100kHz, depending on the device we select. Reading the motor control manual, I discovered th...

Resolved! Software support for the baord EVSPIN32F0251S1

Hello,I would like to build a circuit to drive a three phase BLDC motor and the board EVSPIN32F0251S1 seems to be a choice, but i can't find the software easily. Does anyone know a three phase BLDC firmware project for this board? My build tool is Ke...

WWang.12 by Associate
  • 1221 Views
  • 1 replies
  • 0 kudos

Resolved! Encoder index / HRTIM in H7 or F7

Hi there,​1.My first question is about encoder index.​I know that encoder index(so called Z pulse) is applicable in G4 series. (RM0440 1,109 pages)​However I can't find that feature in any of H7 and F7 sereis.​2.I know that the maximum resolution of ...

Resolved! Motor profiles and MIGE motors

I purchased two different ST controller boards:B-G431B-ESC1NUCLEO-G431RB and X-NUCLEO-IHM16M1I also have two motors:MIGE 80ST-M04025MIGE 130ST-M10010I've tried to profile the motors using the ST Motor Profiler but it always errors with "Profiling tak...

0693W000000UCV6QAO.png
SPiet.1 by Associate
  • 1392 Views
  • 1 replies
  • 0 kudos

Resolved! Support for Hall Sensor control?

Anyone know if the MCWB will include hall sensor control sometime soon? I don't see anything and the various documents are out of date and contradictory.

GBuke.1 by Associate
  • 1339 Views
  • 1 replies
  • 0 kudos

Resolved! Changing Over Current Protection Comparator threshold does not change the Standby 1 and 2 outputs accordingly in the code

I'm currently trying to spin a motor using the STEVAL_SPIN3201 and the motor control workbench and when I add a small load I get the overcurrent fault. After some research in the source code I realised that the OCCOMP was indeed overcurrenting with t...

0693W000000TglqQAC.png 0693W000000Tgm0QAC.png 0693W000000TglvQAC.png
PBela.1 by Associate II
  • 2393 Views
  • 3 replies
  • 3 kudos