STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1716 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9546 Views
  • 5 replies
  • 3 kudos

Anyone else having problems with Nucleo F302R8 with the IHM08M1 driver board to run a motor using the X-Cube SPN8 6-step algorithm?

We are currently using a Nucleo F302R8 with the IHM08M1 driver board and the Bull Running BR2804 motor provided with the development kit. We are using ST's X-Cube SPN8, 6-step software and compiled it, unmodified, with Keil MDK 5. Unfortunately, the ...

MBlan.1 by Associate
  • 1167 Views
  • 3 replies
  • 0 kudos

Resolved! Where can I download MC SDK V4.3?

I am having the P-Nucleo IHM001. I am trying to generate code using ST Motor Control Workbench, but after building and dumping the code in the controller, the motor is not spinning and two faults are showing up:FOC faultSoftware errorI want to try ol...

PPati.1 by Associate II
  • 3484 Views
  • 6 replies
  • 0 kudos

Resolved! Why is the STEVAL-SPIN3201 limited to 15 Arms?

Hi, I read in the Data Brief of the STEVAL-SPIN3201 module that it can ouput up to 15 Arms of current but I can't find in the schematic why that it. The mosfet used on the board (STD140N6F7) seems capable of higher current output.We want to port the ...

PBela.1 by Associate II
  • 1266 Views
  • 1 replies
  • 0 kudos

Resolved! Encoder "reverse counting direction" checkbox not working in ST MC Workbench 5.4.3. What am I missing?

Hi all,I have been pulling my hair out trying different ways to reverse my encoder counting direction.The checkbox "reverse counting direction" in Speed Sensing section does not seem to make any difference. I am using Attolic TrueSTUDIO IDE, and the ...

Frakk by Associate II
  • 3096 Views
  • 5 replies
  • 0 kudos

Resolved! how to turn off both complementary pwm at the same time

I am using STM32F4 to drive a 3 phase BLDC motor and i'm using TIM1 peripheral to generate 6-step PWM(complementary pwm) but when i change the configuration and i disable 1 channel it takes some time to go low which causing problems (you can check th...

mboua by Associate
  • 2639 Views
  • 3 replies
  • 0 kudos

Resolved! Does MC_SDK require the use of coprocessor?

We are developing an application to drive dual PMSM motors with STM32H745 and FOC algorithms and resolver sensor. The inner current loops are executed at 10 kHz, PWM carrier frequency is set to 20 kHz. Is it feasible o run the entire application code...

LZhu.1 by Associate
  • 1240 Views
  • 1 replies
  • 0 kudos

Resolved! Recommended setup for small motor position control?

I have a small BLDC motor with magnetic encoder (like this one https://www.aliexpress.com/item/33053552345.html) and would like to set up a position control. The NUCLEO-IHM03 comes pretty close https://www.st.com/content/st_com/en/products/evaluatio...

Martin294 by Associate III
  • 5352 Views
  • 8 replies
  • 0 kudos