STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1725 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4873 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9558 Views
  • 5 replies
  • 3 kudos

ST Motor Control Workbench is not generating code

Hello.I am tring to generate my project on st motor control workbench. I clicked to generate button and I choose the version of my CubeMX and TrueStudio. But workbench stuck in generation phase. Here is the window that I've seen for 20 minutes. What ...

0693W000001pfHnQAI.jpg
İDuma.1 by Associate
  • 1200 Views
  • 2 replies
  • 0 kudos

STM32 Hall Sensor Interface

I had a few questions that I was hoping someone could help clear up. I am trying to just use the interface timer for speed calculations. When I am reading the documentation it states 3 channels are tied together to cause a trigger, what if my encoder...

CFran.1 by Associate II
  • 1530 Views
  • 2 replies
  • 0 kudos

STM32100B-eval or EVSPIN32F0601s1

Hello,May I know how open the board STM32100B-eval or EVSPIN32F0601s1? I mean the FOC on either of these two boards is established. And the current loop, velocity and position loop are all controlled by PID. I wonder, is it possible that I use the fi...

Shiba by Associate
  • 968 Views
  • 2 replies
  • 0 kudos

Resolved! PID tuning to achieve smoothness at very low speeds

Hi, I am using the NUCLEO-F303RE and NUCLEO-IHM08M1 to drive a maxon 48V DC motor with incremental encoder (1024 counts). I have used the motor profiler and motor control workbench, the PID values automatically generated were completely wrong and the...

0693W000001qcpeQAA.jpg
msingh by Senior
  • 6282 Views
  • 7 replies
  • 0 kudos

MC_GetAlignmentStatusMotor1() never end

HelloI am trying to implement Position control with the latest version 5.4.4 of motor library, but the alignment function never succeeds and this loop has run forever :  while(MC_GetAlignmentStatusMotor1()!=TC_ALIGNMENT_COMPLETED){}I am using quadrat...

JEsca.1 by Associate II
  • 1346 Views
  • 2 replies
  • 0 kudos

Resolved! Hi sir this is rahul yadav working in greenfield control system r & d , sir i am using steval 3202 board sir i want to spin bldc motor with hall sensor i am usinf stspin motor control work bench but motor is doing noise and torque is not up to the mark

what parameter should i enter for hall sensored foc control in motor control work bench any pdf available for hall sensored foc control in motor control work bench 5.2.0 sir problem is motor is spining but torque is less any guidlines avai...

Ryada.1 by Associate II
  • 3663 Views
  • 9 replies
  • 0 kudos